How do I bring/brought up Ethernet interfaces for Main Domain CPSWnG in Linux from SDK Version 9.0 and above?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
From SDK 9.0 Onwards Ethernet drivers for CPSWnG will not be enabled by default in Linux.
We need to add the device-tree overlays to the uEnv.txt file (in boot partition of SD card if SD boot mode is used), as shown below to load the driver in every boot.
name_overlays=ti/<overlay-file-name> OR
name_overlays=<overlay-file-name>
The overlay addition with ti/<overlay> or <overlay> depends upon following from u-boot/include/environment/ti/mmc.env. if ti/ already present like below then use <overlay>, if not, use ti/<overlay>.
For SDK 9.0 and 10.0 it will be ti/<overlay-file-name>
For SDK 9.1 and 9.2 it will be <overlay-file-name>
For Virtual MAC driver:
|
SoC |
Overlay file to use |
|
J7200/DRA821 |
k3-j7200-evm-virt-mac-client.dtbo |
|
J721e/TDA4VM/DRA829 |
k3-j721e-evm-virt-mac-client.dtbo |
|
J784S4/TDA4VH |
k3-j784s4-evm-virt-mac-client.dtbo |
|
SoC |
Command to map firmware binay |
|
J7200/DRA821 |
# ln -s /lib/firmware/ti-eth/j7200/app_remoteswitchcfg_server_strip.xer5f j7200-main-r5f0_0-fw |
|
J721e/TDA4VM/DRA829 |
# ln -s /lib/firmware/ti-eth/j721e/app_remoteswitchcfg_server_strip.xer5f j721e-main-r5f0_0-fw |
|
J784S4/TDA4VH |
# ln -s /lib/firmware/ti-eth/j784s4/app_remoteswitchcfg_server_strip.xer5f j784s4-main-r5f0_0-fw |
For Native Linux Driver:
|
SoC |
MAC Ports Interface |
Overlay file to use |
|
J7200/DRA821 |
QSGMII |
k3-j7200-evm-quad-port-eth-exp.dtbo |
|
J721e/TDA4VM/DRA829 |
RGMII |
k3-j721e-evm-gesi-exp-board.dtbo |
|
J721e/TDA4VM/DRA829 |
QSGMII |
k3-j721e-evm-quad-port-eth-exp.dtbo |
|
J721S2/TDA4VL |
RGMII |
k3-j721s2-evm-gesi-exp-board.dtbo |
|
J784S4/TDA4VH |
QSGMII |
k3-j784s4-evm-quad-port-eth1-exp.dtbo |
|
J784S4/TDA4VH |
USXGMII |
k3-j784s4-evm-usxgmii-exp1-exp2.dtbo |
2. Along with overlay addition, make sure that ETHFW is not loaded in MCU2_0.
a) If vision Apps is used with vision overlay then rebuild vision application by disabling ETHFW. Please refer to vision-apps user guide (from SDK documentation) for more details about build steps and build flags.
b) If vision Apps is not using, we can soft link ipc echo test binary (ipc_echo_test_mcu2_0_release_strip.xer5f from /lib/firmware/ti-ipc/<soc>) to MCU2_0, refer to above ETHFW binary soft link commands
Note:
For enabling 8 ports in case of CPSW9G, we have to manage the device tress files such that to enable all 8 Ports.
Best Regards,
Sudheer