Other Parts Discussed in Thread: TMS320DM6467
We are using TMS320DM6467, Digital Media System-on-Chip (DMSoC).
We have a requirement wherein We need to synchronize the decoded audio and video streams to the 27-MHZ PCR timestamp added by the encoder to the stream.
As we understand, TMS320DM6467 provides a clock reference generator(CRGEN) module which recovers the 27-MHZ system clock from the program clock reference (PCR) value that is detected by the transport stream interface (TSIF) module. We were thinking if we could use the same to acheive our objective. A few doubts that regarding the same:
Can CRGEN be used with multi program streams? We need it to work for multi program streams. Is there any way in which it can be configured to do so? Also, It would be nice If you could point to some other ellaborate doccumentations which explain the usage of CRGEN.
The online doccumentation (http://focus.ti.com/dsp/docs/litabsmultiplefilelist.tsp?sectionId=3&tabId=409&literatureNumber=sprueq1&docCategoryId=6&familyId=1506) does not state anything about this.