This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ezdsp c5515 HOST interface (RTDX, UART, USB)

Hi!

I am trying to interface PC to the ezdsp c5515 usb stick using the following 3 interfaces.

1. USB port

    I was ableo to communicate with PC in Full Speed mode (USB DMA example in CSL 2.5).

   Still working on High Speed mode.  Any one tell me how to make USB DMA example work in

   high speed mode?

2. USB (JTAG) port (RTDX)

    With DSK6713, examples were provided. Any examples for ezdsp c5515?

   I am seeking for RTDX examples for Visual C++ 6.0 platform.

3. UART port

   Is it possible to compose an UART port in ezdsp C5515?  If Yes, please tell me where to start.

 

Thanks and regards

HG KIM

 

 

1