Other Parts Discussed in Thread: AM62A7
Following are some questions regarding the use of NAND flash via the AM62A GPMC. The use case is not for booting, but for additional file/data storage. The motivation of these questions is the fit of parallel NAND as better performance than QSPI NAND, and lower density/cost options than eMMC.
So would like to understand performance, and availability of any examples/demos.
- Do any demos exist for GMPC raw NAND?
- If so, please share design details, including NAND manufacturer part number, GPMC config, and any timing related info
- The AM62A TRM has diagrams with 8-bit usage. Please confirm 16-bit is supported as well. Likewise, any demo/support information with 16-bit will be appreciated.
- Any relevant performance benchmark data will be very useful
Thanks,
Eric