Part Number: SK-AM62A-LP
Other Parts Discussed in Thread: CC3301,
Hello,
I have an m.2 key E module from Laird that use an Infineon (Cypress) CYW4373E module see details here.
We have the version 453-00049 that use usb/usb for wifi and ble
I use the lastest sdk (9.0). Can you tell me if the driver is included in the image please ?
As i understand, the cypress soc use brcmfmac driver. On the card i did this
root@am62axx-evm:/sys/bus/pci# zcat /proc/config.gz | grep -i brcmfmac CONFIG_BRCMFMAC=m CONFIG_BRCMFMAC_PROTO_BCDC=y CONFIG_BRCMFMAC_SDIO=y # CONFIG_BRCMFMAC_USB is not set # CONFIG_BRCMFMAC_PCIE is not set
I suppose i need to build the usb module for the kernel ?
or do i need to use this backport of laird : https://www.lairdconnect.com/documentation/application-note-petalinux-software-integration-60-series-and-lwb-series
Otherwise if i order the sdio/uart module 453-00048 it will work without the need to build kernel module ?
Regards