Other Parts Discussed in Thread: OMAP-L138, OMAPL138
Can anyone please Help?
Using ti-dvsdk_omapl138-evm_4_02_00_06 SDK located in my /home/user/ti-dvsdk_omapl138-evm_4_02_00_06 with its linux-2.6.33-rc4-psp03.20.00.14.sdk., located in /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/ linux-2.6.33-rc4-psp03.20.00.14.sdk
On OMAP-L138 Logic P.D. Zoom evaluation board.
I also have CodeSourcery tools and its Sourcery_G++_Lite/arm-none-linux-gnueabi tools (i.e. gcc and ld) in my /home/user directory /home/user/CodeSourcery/Sourcery_G++_Lite/arm-none-linux-gnueabi/bin.
I am trying to build the USB WiFi driver for a Ralink rt3070 part.
The driver firmware provided by the manufacture is attached.
I have extracted 2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO.tar to a folder under
/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/ wyfy... so it looks like this
/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO> ls -l
total 96
drwxr-xr-x 2 user user 4096 2011-01-06 20:18 chips
drwxr-xr-x 2 user user 4096 2011-08-03 14:14 common
drwxr-xr-x 5 user user 4096 2011-01-06 20:20 include
-rwxrwxrwx 1 user user 14819 2011-01-06 20:18 iwpriv_usage.txt
-rw-r--r-- 1 user user 14343 2011-08-03 10:10 Makefile
drwxrwxrwx 3 user user 4096 2011-01-06 20:18 os
-rw-r--r-- 1 user user 13527 2011-01-06 20:18 README_STA_usb
-rwxrwxrwx 1 user user 613 2011-01-06 20:18 RT2870STACard.dat
-rwxrwxrwx 1 user user 1118 2011-01-06 20:18 RT2870STA.dat
drwxr-xr-x 2 user user 4096 2011-01-06 20:18 sta
-rwxrwxrwx 1 user user 14253 2011-01-06 20:18 sta_ate_iwpriv_usage.txt
drwxr-xr-x 2 user user 4096 2011-08-03 21:06 tools
In the firmware package is README_STA_usb file describing what to do to build it.
I have made a attempt to carry out step 2 and 3 i.e.
----------------------------------------------------
2> In Makefile
set the "MODE = STA" in Makefile and chose the TARGET to Linux by set "TARGET = LINUX"
define the linux kernel source include file path LINUX_SRC
modify to meet your need.
3> In os/linux/config.mk
define the GCC and LD of the target machine
define the compiler flags CFLAGS
modify to meet your need.
** Build for being controlled by NetworkManager or wpa_supplicant wext functions
Please set 'HAS_WPA_SUPPLICANT=y' and 'HAS_NATIVE_WPA_SUPPLICANT_SUPPORT=y'.
=> #>cd wpa_supplicant-x.x
=> #>./wpa_supplicant -Dwext -ira0 -c wpa_supplicant.conf -d
** Build for being controlled by WpaSupplicant with Ralink Driver
Please set 'HAS_WPA_SUPPLICANT=y' and 'HAS_NATIVE_WPA_SUPPLICANT_SUPPORT=n'.
=> #>cd wpa_supplicant-0.5.7
=> #>./wpa_supplicant -Dralink -ira0 -c wpa_supplicant.conf -d
----------------------------------------------------
In step 2 I have created a OMAP_L138 PLATFORM definition and “think” I have the correct defines as follows...
PLATFORM = OMAP_L138
…............
…...........
…...........
ifeq ($(PLATFORM),OMAP_L138)
LINUX_SRC = /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk
CROSS_COMPILE = /home/user/CodeSourcery/Sourcery_G++_Lite/bin/
endif
in the /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/makefile.
Note: the reason I say “think” concernes how I defined LINUX_SRC as
LINUX_SRC = /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk see comment below...
In step 3 I have created / changed the followin
changed
# CC := $(CROSS_COMPILE)gcc
# LD := $(CROSS_COMPILE)ld
CC := $(CROSS_COMPILE)arm-none-linux-gnueabi-gcc
LD := $(CROSS_COMPILE)arm-none-linux-gnueabi-ld
created
ifeq ($(PLATFORM),OMAP_L138)
EXTRA_CFLAGS := -v -Wfatal-errors -I$(RT28xx_DIR)/include -I/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk/arch/arm/include -I/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/cgt6x_6_1_14/include $(WFLAGS)
endif
Note: I'm not at all sure about
-I/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/cgt6x_6_1_14/include
Or if any of the -I includes are correct? However I do manage to get ferther along in the build / make process with them included.
I also included some echo, warning messages in the make file to verify my defines. The will be seen in the output from make. Sorry this is a long output but maybe a clue for someone to help etc.
[linux-devkit]:~/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO> make ARCH=arm
make -C tools
make[1]: Entering directory `/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/tools'
gcc -g bin2h.c -o bin2h
make[1]: Leaving directory `/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/tools'
/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/tools/bin2h
Making Bin2h
Exiting bin2h make
Makefile:372: pLATFORME is OMAP_L138
Makefile:372: LINUX_SRC is /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk
Makefile:372: CROSS_COMPILE is /home/user/CodeSourcery/Sourcery_G++_Lite/bin/
Makefile:372: RT28xx_DIR is /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO
cp -f os/linux/Makefile.6 /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/os/linux/Makefile
make -C /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk SUBDIRS=/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/os/linux modules
make[1]: /home/user/CodeSourcery/Sourcery_G++_Lite/bin/gcc: Command not found
make[1]: Entering directory `/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk'
CC [M] /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/os/linux/../../common/crypt_md5.o
Using built-in specs.
Target: arm-none-linux-gnueabi
Configured with: /scratch/mitchell/builds/4.3-arm-none-linux-gnueabi-respin/src/gcc-4.3/configure --build=i686-pc-linux-gnu --host=i686-pc-linux-gnu --target=arm-none-linux-gnueabi --enable-threads --disable-libmudflap --disable-libssp --disable-libstdcxx-pch --with-gnu-as --with-gnu-ld --with-specs='%{funwind-tables|fno-unwind-tables|mabi=*|ffreestanding|nostdlib:;:-funwind-tables}' --enable-languages=c,c++ --enable-shared --enable-symvers=gnu --enable-__cxa_atexit --with-pkgversion='Sourcery G++ Lite 2009q1-203' --with-bugurl=https://support.codesourcery.com/GNUToolchain/ --disable-nls --prefix=/opt/codesourcery --with-sysroot=/opt/codesourcery/arm-none-linux-gnueabi/libc --with-build-sysroot=/scratch/mitchell/builds/4.3-arm-none-linux-gnueabi-respin/lite/install/arm-none-linux-gnueabi/libc --with-gmp=/scratch/mitchell/builds/4.3-arm-none-linux-gnueabi-respin/lite/obj/host-libs-2009q1-203-arm-none-linux-gnueabi-i686-pc-linux-gnu/usr --with-mpfr=/scratch/mitchell/builds/4.3-arm-none-linux-gnueabi-respin/lite/obj/host-libs-2009q1-203-arm-none-linux-gnueabi-i686-pc-linux-gnu/usr --disable-libgomp --enable-poison-system-directories --with-build-time-tools=/scratch/mitchell/builds/4.3-arm-none-linux-gnueabi-respin/lite/install/arm-none-linux-gnueabi/bin --with-build-time-tools=/scratch/mitchell/builds/4.3-arm-none-linux-gnueabi-respin/lite/install/arm-none-linux-gnueabi/bin
Thread model: posix
gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203)
COLLECT_GCC_OPTIONS='-nostdinc' '-isystem' '-I/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk/arch/arm/include' '-Iinclude' '-include' 'include/generated/autoconf.h' '-D__KERNEL__' '-mlittle-endian' '-Iarch/arm/mach-davinci/include' '-Wundef' '-fno-strict-aliasing' '-fno-common' '-Werror-implicit-function-declaration' '-Wno-format-security' '-fno-delete-null-pointer-checks' '-Os' '-mapcs' '-mno-sched-prolog' '-mabi=aapcs-linux' '-mno-thumb-interwork' '-D__LINUX_ARM_ARCH__=5' '-march=armv4t' '-mtune=arm9tdmi' '-msoft-float' '-Uarm' '-fno-omit-frame-pointer' '-fno-optimize-sibling-calls' '-v' '-Wfatal-errors' '-I/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/include' '-I/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk/arch/arm/include' '-I/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/cgt6x_6_1_14/include' '-DAGGREGATION_SUPPORT' '-DPIGGYBACK_SUPPORT' '-DWMM_SUPPORT' '-DLINUX' '-Wall' '-Wstrict-prototypes' '-Wno-trigraphs' '-DSYSTEM_LOG_SUPPORT' '-DRT28xx_MODE=STA' '-DCHIPSET=3070' '-DRESOURCE_PRE_ALLOC' '-DCONFIG_STA_SUPPORT' '-DDBG' '-DDOT11_N_SUPPORT' '-DDOT11N_DRAFT3' '-DSTATS_COUNT_SUPPORT' '-DRTMP_MAC_USB' '-DRT30xx' '-DRT3070' '-DRTMP_USB_SUPPORT' '-DRTMP_TIMER_TASK_SUPPORT' '-DRTMP_RF_RW_SUPPORT' '-DRTMP_EFUSE_SUPPORT' '-DSPECIFIC_VCORECAL_SUPPORT' '-DMODULE' '-DKBUILD_STR(s)=#s' '-DKBUILD_BASENAME=KBUILD_STR(crypt_md5)' '-DKBUILD_MODNAME=KBUILD_STR(rt3070sta)' '-c' '-o' '/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/os/linux/../../common/.tmp_crypt_md5.o'
/home/user/CodeSourcery/Sourcery_G++_Lite/bin/../libexec/gcc/arm-none-linux-gnueabi/4.3.3/cc1 -quiet -nostdinc -v -Iinclude -Iarch/arm/mach-davinci/include -I/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/include -I/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk/arch/arm/include -I/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/cgt6x_6_1_14/include -imultilib armv4t -iprefix /home/user/CodeSourcery/Sourcery_G++_Lite/bin/../lib/gcc/arm-none-linux-gnueabi/4.3.3/ -isysroot /home/user/CodeSourcery/Sourcery_G++_Lite/bin/../arm-none-linux-gnueabi/libc -D__KERNEL__ -D__LINUX_ARM_ARCH__=5 -Uarm -DAGGREGATION_SUPPORT -DPIGGYBACK_SUPPORT -DWMM_SUPPORT -DLINUX -DSYSTEM_LOG_SUPPORT -DRT28xx_MODE=STA -DCHIPSET=3070 -DRESOURCE_PRE_ALLOC -DCONFIG_STA_SUPPORT -DDBG -DDOT11_N_SUPPORT -DDOT11N_DRAFT3 -DSTATS_COUNT_SUPPORT -DRTMP_MAC_USB -DRT30xx -DRT3070 -DRTMP_USB_SUPPORT -DRTMP_TIMER_TASK_SUPPORT -DRTMP_RF_RW_SUPPORT -DRTMP_EFUSE_SUPPORT -DSPECIFIC_VCORECAL_SUPPORT -DMODULE -DKBUILD_STR(s)=#s -DKBUILD_BASENAME=KBUILD_STR(crypt_md5) -DKBUILD_MODNAME=KBUILD_STR(rt3070sta) -isystem -I/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk/arch/arm/include -include include/generated/autoconf.h -MD /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/os/linux/../../common/.crypt_md5.o.d /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/os/linux/../../common/crypt_md5.c -quiet -dumpbase crypt_md5.c -mlittle-endian -mapcs -mno-sched-prolog -mabi=aapcs-linux -mno-thumb-interwork -march=armv4t -mtune=arm9tdmi -msoft-float -auxbase-strip /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/os/linux/../../common/.tmp_crypt_md5.o -Os -Wundef -Werror-implicit-function-declaration -Wno-format-security -Wfatal-errors -Wall -Wstrict-prototypes -Wno-trigraphs -version -fno-strict-aliasing -fno-common -fno-delete-null-pointer-checks -fno-omit-frame-pointer -fno-optimize-sibling-calls -o /tmp/cccVBZrK.s
ignoring nonexistent directory "-I/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk/arch/arm/include"
#include "..." search starts here:
#include <...> search starts here:
include
arch/arm/mach-davinci/include
/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/include
/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk/arch/arm/include
/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/cgt6x_6_1_14/include
/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/linux-devkit//arm-none-linux-gnueabi/usr/include
.
End of search list.
GNU C (Sourcery G++ Lite 2009q1-203) version 4.3.3 (arm-none-linux-gnueabi)
compiled by GNU C version 4.3.2, GMP version 4.2.4, MPFR version 2.3.2.
GGC heuristics: --param ggc-min-expand=63 --param ggc-min-heapsize=63653
Compiler executable checksum: ff2e25870db5a86cad0a49ae0451c7d1
In file included from include/linux/mmzone.h:20,
from include/linux/gfp.h:4,
from include/linux/kmod.h:22,
from include/linux/module.h:13,
from /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/include/os/rt_linux.h:31,
from /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/include/rtmp_os.h:44,
from /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/include/rtmp_comm.h:60,
from /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/include/rt_config.h:33,
from /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/os/linux/../../common/crypt_md5.c:28:
include/asm/page.h:9:2: error: #error need to prove a real asm/page.h
In file included from include/linux/ktime.h:25,
from include/linux/timer.h:5,
from include/linux/workqueue.h:8,
from include/linux/slub_def.h:11,
from include/linux/slab.h:162,
from include/linux/percpu.h:5,
from include/asm/local.h:4,
from include/linux/module.h:20,
from /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/include/os/rt_linux.h:31,
from /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/include/rtmp_os.h:44,
from /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/include/rtmp_comm.h:60,
from /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/include/rt_config.h:33,
from /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/os/linux/../../common/crypt_md5.c:28:
include/linux/jiffies.h:257:31: warning: "CLOCK_TICK_RATE" is not defined
include/linux/jiffies.h:257:31: warning: "CLOCK_TICK_RATE" is not defined
include/linux/jiffies.h:257:31: error: division by zero in #if
include/linux/jiffies.h:257:31: warning: "CLOCK_TICK_RATE" is not defined
include/linux/jiffies.h:257:31: warning: "CLOCK_TICK_RATE" is not defined
include/linux/jiffies.h:257:31: error: division by zero in #if
include/linux/jiffies.h:257:31: warning: "CLOCK_TICK_RATE" is not defined
include/linux/jiffies.h:257:31: warning: "CLOCK_TICK_RATE" is not defined
include/linux/jiffies.h:257:31: error: division by zero in #if
include/linux/jiffies.h:257:31: error: division by zero in #if
include/linux/jiffies.h:257:31: warning: "CLOCK_TICK_RATE" is not defined
include/linux/jiffies.h:257:31: warning: "CLOCK_TICK_RATE" is not defined
include/linux/jiffies.h:257:31: error: division by zero in #if
include/linux/jiffies.h:257:31: warning: "CLOCK_TICK_RATE" is not defined
include/linux/jiffies.h:257:31: warning: "CLOCK_TICK_RATE" is not defined
include/linux/jiffies.h:257:31: error: division by zero in #if
include/linux/jiffies.h:257:31: warning: "CLOCK_TICK_RATE" is not defined
include/linux/jiffies.h:257:31: warning: "CLOCK_TICK_RATE" is not defined
include/linux/jiffies.h:257:31: error: division by zero in #if
include/linux/jiffies.h:257:31: error: division by zero in #if
include/linux/jiffies.h:257:31: warning: "CLOCK_TICK_RATE" is not defined
include/linux/jiffies.h:257:31: warning: "CLOCK_TICK_RATE" is not defined
include/linux/jiffies.h:257:31: error: division by zero in #if
include/linux/jiffies.h:257:31: warning: "CLOCK_TICK_RATE" is not defined
include/linux/jiffies.h:257:31: warning: "CLOCK_TICK_RATE" is not defined
include/linux/jiffies.h:257:31: error: division by zero in #if
include/linux/jiffies.h:257:31: warning: "CLOCK_TICK_RATE" is not defined
include/linux/jiffies.h:257:31: warning: "CLOCK_TICK_RATE" is not defined
include/linux/jiffies.h:257:31: error: division by zero in #if
include/linux/jiffies.h:257:31: warning: "CLOCK_TICK_RATE" is not defined
include/linux/jiffies.h:257:31: warning: "CLOCK_TICK_RATE" is not defined
include/linux/jiffies.h:257:31: error: division by zero in #if
include/linux/jiffies.h:257:31: warning: "CLOCK_TICK_RATE" is not defined
include/linux/jiffies.h:257:31: warning: "CLOCK_TICK_RATE" is not defined
include/linux/jiffies.h:257:31: error: division by zero in #if
include/linux/jiffies.h:257:31: warning: "CLOCK_TICK_RATE" is not defined
include/linux/jiffies.h:257:31: warning: "CLOCK_TICK_RATE" is not defined
include/linux/jiffies.h:257:31: error: division by zero in #if
include/linux/jiffies.h:257:31: error: division by zero in #if
In file included from include/linux/mm.h:39,
from include/asm/cacheflush.h:5,
from include/asm/io.h:15,
from include/linux/io.h:22,
from include/linux/pci.h:54,
from /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/include/os/rt_linux.h:41,
from /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/include/rtmp_os.h:44,
from /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/include/rtmp_comm.h:60,
from /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/include/rt_config.h:33,
from /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/os/linux/../../common/crypt_md5.c:28:
include/asm/pgtable.h: In function 'ptep_set_wrprotect':
include/asm/pgtable.h:98: error: implicit declaration of function 'set_pte_at'
compilation terminated due to -Wfatal-errors.
make[2]: *** [/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/os/linux/../../common/crypt_md5.o] Error 1
make[1]: *** [_module_/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/os/linux] Error 2
make[1]: Leaving directory `/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk'
make: *** [LINUX] Error 2
This error above “include/asm/page.h:9:2: error: #error need to prove a real asm/page.h”
leads me to beleave I have a path or define or include incorrect for my sdk / environment or ?
This is the reason for the “Note: the reason I say “think” concerns how I defined LINUX_SRC as
LINUX_SRC = /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk “
Also I question issuing make ARCH=arm
with the ARCH=arm, note: if I do not use the ARCH=arm I get the following
[linux-devkit]:~/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO> make
make -C tools
make[1]: Entering directory `/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/tools'
gcc -g bin2h.c -o bin2h
make[1]: Leaving directory `/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/tools'
/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/tools/bin2h
Making Bin2h
Exiting bin2h make
Makefile:372: pLATFORME is OMAP_L138
Makefile:372: LINUX_SRC is /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk
Makefile:372: CROSS_COMPILE is /home/user/CodeSourcery/Sourcery_G++_Lite/bin/
Makefile:372: RT28xx_DIR is /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO
cp -f os/linux/Makefile.6 /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/os/linux/Makefile
make -C /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk SUBDIRS=/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/os/linux modules
make[1]: /home/user/CodeSourcery/Sourcery_G++_Lite/bin/gcc: Command not found
make[1]: Entering directory `/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk'
CC [M] /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/os/linux/../../common/crypt_md5.o
Using built-in specs.
Target: arm-none-linux-gnueabi
Configured with: /scratch/mitchell/builds/4.3-arm-none-linux-gnueabi-respin/src/gcc-4.3/configure --build=i686-pc-linux-gnu --host=i686-pc-linux-gnu --target=arm-none-linux-gnueabi --enable-threads --disable-libmudflap --disable-libssp --disable-libstdcxx-pch --with-gnu-as --with-gnu-ld --with-specs='%{funwind-tables|fno-unwind-tables|mabi=*|ffreestanding|nostdlib:;:-funwind-tables}' --enable-languages=c,c++ --enable-shared --enable-symvers=gnu --enable-__cxa_atexit --with-pkgversion='Sourcery G++ Lite 2009q1-203' --with-bugurl=https://support.codesourcery.com/GNUToolchain/ --disable-nls --prefix=/opt/codesourcery --with-sysroot=/opt/codesourcery/arm-none-linux-gnueabi/libc --with-build-sysroot=/scratch/mitchell/builds/4.3-arm-none-linux-gnueabi-respin/lite/install/arm-none-linux-gnueabi/libc --with-gmp=/scratch/mitchell/builds/4.3-arm-none-linux-gnueabi-respin/lite/obj/host-libs-2009q1-203-arm-none-linux-gnueabi-i686-pc-linux-gnu/usr --with-mpfr=/scratch/mitchell/builds/4.3-arm-none-linux-gnueabi-respin/lite/obj/host-libs-2009q1-203-arm-none-linux-gnueabi-i686-pc-linux-gnu/usr --disable-libgomp --enable-poison-system-directories --with-build-time-tools=/scratch/mitchell/builds/4.3-arm-none-linux-gnueabi-respin/lite/install/arm-none-linux-gnueabi/bin --with-build-time-tools=/scratch/mitchell/builds/4.3-arm-none-linux-gnueabi-respin/lite/install/arm-none-linux-gnueabi/bin
Thread model: posix
gcc version 4.3.3 (Sourcery G++ Lite 2009q1-203)
COLLECT_GCC_OPTIONS='-nostdinc' '-isystem' '-I/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk/arch/x86/include' '-Iinclude' '-include' 'include/generated/autoconf.h' '-D__KERNEL__' '-Wundef' '-fno-strict-aliasing' '-fno-common' '-Werror-implicit-function-declaration' '-Wno-format-security' '-fno-delete-null-pointer-checks' '-Os' '-m64' '-mno-red-zone' '-mcmodel=kernel' '-maccumulate-outgoing-args' '-pipe' '-Wno-sign-compare' '-fno-asynchronous-unwind-tables' '-fno-omit-frame-pointer' '-fno-optimize-sibling-calls' '-v' '-Wfatal-errors' '-I/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/include' '-I/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk/arch/arm/include' '-I/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/cgt6x_6_1_14/include' '-DAGGREGATION_SUPPORT' '-DPIGGYBACK_SUPPORT' '-DWMM_SUPPORT' '-DLINUX' '-Wall' '-Wstrict-prototypes' '-Wno-trigraphs' '-DSYSTEM_LOG_SUPPORT' '-DRT28xx_MODE=STA' '-DCHIPSET=3070' '-DRESOURCE_PRE_ALLOC' '-DCONFIG_STA_SUPPORT' '-DDBG' '-DDOT11_N_SUPPORT' '-DDOT11N_DRAFT3' '-DSTATS_COUNT_SUPPORT' '-DRTMP_MAC_USB' '-DRT30xx' '-DRT3070' '-DRTMP_USB_SUPPORT' '-DRTMP_TIMER_TASK_SUPPORT' '-DRTMP_RF_RW_SUPPORT' '-DRTMP_EFUSE_SUPPORT' '-DSPECIFIC_VCORECAL_SUPPORT' '-DMODULE' '-DKBUILD_STR(s)=#s' '-DKBUILD_BASENAME=KBUILD_STR(crypt_md5)' '-DKBUILD_MODNAME=KBUILD_STR(rt3070sta)' '-c' '-o' '/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/os/linux/../../common/.tmp_crypt_md5.o' '-funwind-tables'
/home/user/CodeSourcery/Sourcery_G++_Lite/bin/../libexec/gcc/arm-none-linux-gnueabi/4.3.3/cc1 -quiet -nostdinc -v -Iinclude -I/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/include -I/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk/arch/arm/include -I/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/cgt6x_6_1_14/include -iprefix /home/user/CodeSourcery/Sourcery_G++_Lite/bin/../lib/gcc/arm-none-linux-gnueabi/4.3.3/ -isysroot /home/user/CodeSourcery/Sourcery_G++_Lite/bin/../arm-none-linux-gnueabi/libc -D__KERNEL__ -DAGGREGATION_SUPPORT -DPIGGYBACK_SUPPORT -DWMM_SUPPORT -DLINUX -DSYSTEM_LOG_SUPPORT -DRT28xx_MODE=STA -DCHIPSET=3070 -DRESOURCE_PRE_ALLOC -DCONFIG_STA_SUPPORT -DDBG -DDOT11_N_SUPPORT -DDOT11N_DRAFT3 -DSTATS_COUNT_SUPPORT -DRTMP_MAC_USB -DRT30xx -DRT3070 -DRTMP_USB_SUPPORT -DRTMP_TIMER_TASK_SUPPORT -DRTMP_RF_RW_SUPPORT -DRTMP_EFUSE_SUPPORT -DSPECIFIC_VCORECAL_SUPPORT -DMODULE -DKBUILD_STR(s)=#s -DKBUILD_BASENAME=KBUILD_STR(crypt_md5) -DKBUILD_MODNAME=KBUILD_STR(rt3070sta) -isystem -I/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk/arch/x86/include -include include/generated/autoconf.h -MD /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/os/linux/../../common/.crypt_md5.o.d /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/os/linux/../../common/crypt_md5.c -quiet -dumpbase crypt_md5.c -m64 -mno-red-zone -mcmodel=kernel -maccumulate-outgoing-args -auxbase-strip /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/os/linux/../../common/.tmp_crypt_md5.o -Os -Wundef -Werror-implicit-function-declaration -Wno-format-security -Wno-sign-compare -Wfatal-errors -Wall -Wstrict-prototypes -Wno-trigraphs -version -fno-strict-aliasing -fno-common -fno-delete-null-pointer-checks -fno-asynchronous-unwind-tables -fno-omit-frame-pointer -fno-optimize-sibling-calls -funwind-tables -o - |
/home/user/CodeSourcery/Sourcery_G++_Lite/bin/../lib/gcc/arm-none-linux-gnueabi/4.3.3/../../../../arm-none-linux-gnueabi/bin/as -v -Iinclude -I/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/include -I/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk/arch/arm/include -I/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/cgt6x_6_1_14/include -meabi=5 -o /home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/os/linux/../../common/.tmp_crypt_md5.o
GNU assembler version 2.19.51 (arm-none-linux-gnueabi) using BFD version (Sourcery G++ Lite 2009q1-203) 2.19.51.20090205
cc1: error: unrecognized command line option "-m64"
cc1: error: unrecognized command line option "-mno-red-zone"
cc1: error: unrecognized command line option "-mcmodel=kernel"
cc1: error: unrecognized command line option "-maccumulate-outgoing-args"
ignoring nonexistent directory "-I/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk/arch/x86/include"
#include "..." search starts here:
#include <...> search starts here:
include
/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/include
/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk/arch/arm/include
/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/cgt6x_6_1_14/include
/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/linux-devkit//arm-none-linux-gnueabi/usr/include
.
End of search list.
GNU C (Sourcery G++ Lite 2009q1-203) version 4.3.3 (arm-none-linux-gnueabi)
compiled by GNU C version 4.3.2, GMP version 4.2.4, MPFR version 2.3.2.
GGC heuristics: --param ggc-min-expand=63 --param ggc-min-heapsize=63653
make[2]: *** [/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/os/linux/../../common/crypt_md5.o] Error 1
make[1]: *** [_module_/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/wyfy/2011_0107_RT3070_RT3370_Linux_STA_v2.5.0.1_DPO/os/linux] Error 2
make[1]: Leaving directory `/home/user/ti-dvsdk_omapl138-evm_4_02_00_06/psp/linux-2.6.33-rc4-psp03.20.00.14.sdk'
make: *** [LINUX] Error 2
cc1: error: unrecognized command line option "-m64"
cc1: error: unrecognized command line option "-mno-red-zone"
Set up for some kind of AMD x86-64 GCC options dont know?
Again, sorry for the long post, and the -v flag to GCC but I am trying to provide as much information as possible so maybe someone can help me.
Thanks all !!
Brian