This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VH-Q1: DPHY

Part Number: TDA4VH-Q1


We encountered a problem in DPHY signal simulation and wanted to ask: when using the IBIS model of TDA4 as the output, the amplitude of the signal is more than 360mV specified by the DPHY signal, and the high level reaches 500mV.我们在DPHY信号仿真当中遇到一个问题想请教:当使用TDA4的IBIS模型作为输出端的时候,信号的幅值是超过DPHY信号规定的360mV的,高电平达到500mV,想请教一下这个如何优化?

以下是信号波形,使用的IO名称是dphy_out_2.5gbps

Below is the signal waveform, using the IO name dphy_out_2.5gbps