Part Number: PROCESSOR-SDK-AM62X
Hi TI
The customer ran the cyclictest program to check the performance of the RT Linux SDK,
A 1 ms control cycle is required to control the robot, and the stress test was conducted with Core3 assigned as a separate process.
If there is no load, there is no problem even if it is operated for more than 8 hours,
If you apply stress, the delay time is longer in about 20 minutes, causing problems.
I would like to ask if there is a separate test method or a solution to the delay time so that the tasks assigned to CORE3 do not cause delay time.
I am attaching their test procedures and results.
Please give me some advice.
Thanks.
Regards,
Jack