Hi E2E'rs
There's probably a page detailing this however ..... I can't find it..
If the c6748 & OMAPL138 are capable of running at 456MHz what is limiting the OMAPL138 SOM-M1 from running at that speed ?
If the limitation is related to the usage of revision 1 OMAPL138 silicon is there a roadmap showing
1 : What additional revisions are available for the OMAPL138. What is the operating speed for each revision, any limiations?
2 : If new revisions of the OMAPL138 are available running at 456MHz are these to be incorporated onto OMAPL138 SOM-M1 - if so roadmap and limitations ?
3 : From what I have been able to ascertain the 24khz oscillator on the eXperimenter board would not be appropriate to provide a 456MHz core clock that was within timing requirements. Is this board to be re-vamped to support higher speeds ?
4 : If a 24MHz oscillator is not appropriate for a OMAPL138 running at 456MHz what should be used ?
BR
Barry