Other Parts Discussed in Thread: THS8200,
We want to Interface one XGA Analog Monitor with THS8200.
Monitor has resolution of [ 1024 X 768 ] .
We want to use AM6548 processor to generate 24 RGB [ 1024 X768 , [Progressive] data using its Video Port-2 which will be input to THS8200.
THS8200 with its 3 inbuilt DACs generate three analog outputs [R,G,B , 1024 X 768 - Progressive ] signals.
My questions are as below
1> Can Video Port-2 of AM6548 is able to generate 1024 x 768 resolution [Progressive] 24bit RGB data ?
2> Can THS8200 support [ 24bit RGB , 1024 X 768 progressive ] resolution signal as input ?
3> What frequency shall I set at [ VOUT1_PCLK ] clock out pin. to drive my XGA Monitor [1024 x 768 Progressive ] resolution.
4> Can I connect VOUT1_DE pin to FID pin of THS8200 ?
Below is the connection diagram for your information. Kindly confirm if I can use this IC THS8200 for driving my XGA[1024x768] Analog Monitor ?