I would like to inquire whether there is a CPU that satisfies the specifications below.
- CPU for wireless communication module (Wi-Fi) control
- Supports PCIe Gen2.0
- Supports QSPI interface
-Linux OS
- Built-in security program: To prevent copying of internal operating software
- Operation Temp: -40~115℃
- Low price (under $15)
- Does not need to be AEQ-100 (not automotive)