This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

uboot nor flash boot patch

hi i modify some uboot code for 8148 nor flash boot

 

diff --git a/arch/arm/cpu/arm_cortexa8/ti81xx/lowlevel_init.S b/arch/arm/cpu/arm_cortexa8/ti81xx/lowlevel_init.S
index 5de3519..390ce29 100644
--- a/arch/arm/cpu/arm_cortexa8/ti81xx/lowlevel_init.S
+++ b/arch/arm/cpu/arm_cortexa8/ti81xx/lowlevel_init.S
@@ -347,13 +347,14 @@ ocmc0_wait0:
        ldr r5, cm_alwon_ocmc_0_clkctrl_addr
        mov r2, #0x2
        str r2, [r5]
-       /* wait for gpmc enable to settle */
+       /* wait for gpmc enable to settle */
 ocmc0_wait1:
        ldr r2, [r5]
        ands r2, r2, #0x00030000
        cmp r2, #0
        bne ocmc0_wait1

+#ifdef CONFIG_TI816X
        /**** enable ocmc 1 ****/
        /* CLKSTCTRL */
        ldr r5, cm_alwon_ocmc_1_clkstctrl_addr
@@ -376,6 +377,7 @@ ocmc1_wait1:
        cmp r2, #0
        bne ocmc1_wait1

+#endif
 nor_init_start:
        /* gpmc init */
        bl  cpy_nor_gpmc_code /* copy nor gpmc init code to sram */
@@ -398,11 +400,15 @@ s_init_start:
 cm_alwon_ocmc_0_clkstctrl_addr:
        .word CM_ALWON_OCMC_0_CLKSTCTRL
 cm_alwon_ocmc_0_clkctrl_addr:
-       .word CM_ALWON_OCMC_0_CLKCTRL
+       .word CM_ALWON_OCMC_0_CLKCTRL
+#ifdef CONFIG_TI816X
+
 cm_alwon_ocmc_1_clkstctrl_addr:
        .word CM_ALWON_OCMC_1_CLKSTCTRL
+
 cm_alwon_ocmc_1_clkctrl_addr:
        .word CM_ALWON_OCMC_1_CLKCTRL
+#endif
 SRAM_STACK:
        .word (SRAM0_START + SRAM0_SIZE - SRAM_GPMC_STACK_SIZE)
 #else

maybe it will be useful

 

 

  • Hi,

     

    Thank you for your contribution. The NOR boot support in our PSP for DM814x should be available by the GA release (end of October).

    As you said this might be useful in the mean time.

     

    Benoit

    P.S. If this response helps answer your question please mark this post as verified - Thanks