Hi,
I am using LogicPD eXperimenter Kit. From the link, there are 2 ways to flash images into the SPI flash, ie serial flasher and spi flash writer.
http://processors.wiki.ti.com/index.php/GSG:_OMAP-L138_DVEVM_Additional_Procedures
We will have custom hardware eventually which will have NOR flash connected to EMIFA.
Questions:
(1) Is there a serial flasher for NOR flash as well ? It is not mentioned in the link, just wnat to confirm that.
(2) The nor flash writer provided, is it meant only to be used for EVM ? Or it can be used with the custom design with different NOR flash ?
DaVinci-PSP-SDK-03.20.00.14/src/utils/nor-flash-writer-03.20.00.14
(3) If it is not meant to support all the different flash parts, I believe I can base on this code to make modification according to the custome design. Would like to understand from TI, what are the details that I should pay attention when doing this modification ?
rgds,
kc Wong