There is two DSP EVM in our company.One is TMS320C6457,and the other is TMS320C6678. According to SDK,6457 woks in CCSV4,while 6678 works in CCSV5.Can i install CCSv4 and CCSv5 in the same PC and in XP system?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
There is two DSP EVM in our company.One is TMS320C6457,and the other is TMS320C6678. According to SDK,6457 woks in CCSV4,while 6678 works in CCSV5.Can i install CCSv4 and CCSv5 in the same PC and in XP system?
Yes, you can install both. You just want them in separate directories. You can use the default directories if you want because the CCSv4 one will be C:\Program Files\Texas Instruments\ccsv4 and the CCSv5 will be in C:\Program Files\Texas Instruments\Texas Instruments\ccsv5
You're right about the 6678 being supported only in CCSv5, but can you point me to the document that says the 6457 doesn't work with CCSv5? I don't believe that this is the case. I suspect that perhaps what the documentation means is that you need to use _at least_ CCSv4. I think you should be able to use CCSv5 with both. I will verify for you if you can give me this info.
Regards,
Dan