Other Parts Discussed in Thread: AM3505, AM3517
Hi,
I have question about memory selection, the target device is AM3505.
(1)NOR Flash Selection
Is there any selection condition for NOR Flash?
For example, is it necessary to be compatible with Intel P30 and AMD?
(2)DDR2 SDRAM Selection
I'm planning to connect the 266MHz 1GByte DDR2 SDRAM to DDR2 interface(Max 166MHz) of AM3505,
is there any problem?
And is there any 1GByte DDR2 SDRAM which have been used in the past with AM3505?
If there is, will you introduce me the model number?