This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6422: Does AM64x support full AVB functionality?

Part Number: AM6422
Other Parts Discussed in Thread: SK-AM62B-P1, TMDS64EVM

Hi all,

We are planning to buy TMDS64EVM AM64x evalution module and SK-AM62B-P1 Starter Kit EVM with PMIC for AVB development purpose.

But we have few queries and doubts which needs to be clarified, could you please us in clarifying them

From the AVB point of view, just wanted to confirm if the support for the following is available in the cspw/ cpts driver

        IEEE 802.1BA: Audio Video Bridging (AVB) Systems
        IEEE 802.1AS: Timing and Synchronization for Time-Sensitive Applications (gPTP)
        IEEE 802.1Qat: Stream Reservation Protocol (SRP)
        IEEE 802.1Qav: Forwarding and Queuing for Time-Sensitive Streams (FQTSS).

And for IEEE 802.1Qat: Stream Reservation Protocol (SRP) how is 75% stream is reserved for AVB is it configurable through cspw/ cpts driver?