This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need help in development of NDK application in c6424

Hi,

I have a requirement of connecting two c6424 EVM boards in loop back mode and to test a unicast application using the NDK libraries.

Could any one please help me to identify the steps require to port the 6748 client example available with the "nsp_1_00_00_09" package.

Can i use the "ndk_2_20_04_26" package for c6424?

What are the other requirements to write a NDK application like the emac driver available with the "nsp_1_00_00_09" package. Where i can get the same emac driver for c6424 EVm board?.

Regards

Ragesh