Hi,
I get this message when I boot the hardware from SD Card.
Texas Instruments X-Loader 1.4.4ss (Feb 11 2011 - 13:00:32)
Waldo1
Reading boot sector
Loading u-boot.bin from mmc
U-Boot 2010.06 (Aug 05 2011 - 17:12:18)
OMAP3430/3530-GP ES3.1, CPU-OPP2 L3-165MHz
OMAP3 Beagle board + LPDDR/NAND
I2C: ready
DRAM: 256 MiB
NAND: 512 MiB
*** Warning - bad CRC or NAND, using default environment
In: serial
Out: serial
Err: serial
Beagle unknown 0x03
Die ID #3530000400000000040373041501b006
Hit any key to stop autoboot: 10 9 8 7 6 5 4 3 2 1 0
mmc1 is available
reading boot.scr
459 bytes read
Running bootscript from mmc ...
## Executing script at 82000000
reading uImage
2618080 bytes read
***** Kernel: /dev/mmcblk0p1/uImage *****
***** RootFS: /dev/mmcblk0p2 *****
## Booting kernel from Legacy Image at 82000000 ...
Image Name: Linux-2.6.32
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2618016 Bytes = 2.5 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux................................................................................................................................................................... done, booting the kernel.
It is stopped.
Please give me some comments about this.
Best Regards
Eric