Part Number: TMDS64GPEVM
Dear Ti experts,
I'm having problem about data length in encryption and decryption proceses in aes-esb-256(Actualy SA2UL functions).
I couldn't encrypt data more than 256kb.
Is there a way to encrypt and decrypt data larger than 256kb?
As in the decryption part of the aes_ecb_256 example, I try to decrypt the encrypted data read from the OSPI flash in a buffer I allocated on the DDR.
/* Decryption */ /* Function to transfer and receive data buffer */ status = SA2UL_contextProcess(&gSa2ulCtxObj,&FlashReadEncBuf[0], size, FlashReadDecBuf); DebugP_assert(SystemP_SUCCESS == status);
The size argument in third parameter equals the actual size of the file in bytes (e.g. 35840 for 35kb)
But in the decrypt process, I get an error when the size of the data to be decrypted from "FlashReadEncBuf" is larger than 256kb(I tested with 908.56kb) and the application crashes.
According to the debug I did, while decrypting the large "FlashReadEncBuf" buffer, I observed that the following iteration was entered in sa2ul.c and the numChunks value was '0xC'.
(SystemP_SUCCESS == retVal)
{
for(processIterations = 0; processIterations < numChunks;processIterations++)
{
retVal = SA2UL_pushBuffer(pCtxObj,ptrInput, maxLength, ptrOutput);
if(SystemP_SUCCESS == retVal)
{
/* Consider timeout */
while((doneBufAddr != (uint64_t)ptrInput) && ( donedataLen != maxLength) && (doneFlag != (uint8_t)TRUE))
{
retVal = SA2UL_popBuffer(pCtxObj, &doneBufAddr, &donedataLen, &doneFlag);
}
}
ptrInput = ptrInput + ((processIterations + 1) * maxLength);
ptrOutput = ptrOutput + ((processIterations + 1) * maxLength);
}I think there are 2 important points in this part.
1:
For the 908kb of data I was trying to decrypt, I initially allocated two separate 1MB Encryption and Decryption buffers.
However, the buffer addresses pointed to by the "ptrInput" and "ptrOutput" pointers in the function expand well over 1MB.
Therefore I updated the buffer size to 6MB for 908kb data.
2:
In the decryption iteration for the 908kb encrypted buffer, when the "processIterations" loop counter reaches '0x5', the "retVal" value from the "SA2UL_pushBuffer" function returns 'SystemP_FAILURE'.
At this stage of the iteration I found the source of the error in the "SA2UL_pushBuffer" function.
The following function in SA2UL_pushBuffer is causing the error:
/* Check the occupancy of storage queue */
if(SA2UL_getStorageRingOcc(object, attrs->swRingNumInt) < 2u)
{
retVal = SystemP_FAILURE;
}In the "SA2UL_getStorageRingOcc" function, the constant "SA2UL_RING_N_ELEMS" and the variable "object->storageQueueFree" both have the value '8U'.
Since the result of this calculation is 0, the previous function generates an error.
I think there is a size limit in the decryption process.
What is the truth here?
I hope you can help with this problem.
Best regards.
(If you want, I can share a demo project to show what I did.)