This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM36x H.264 encoder error 0x8010 at relatively high bitrates



When the DM36x H.264 encoder is set at a relatively large bitrate

(e.g. 1-10 Mbits/second for QVGA), the encoder frequently

fails with extended error 0x8010 (IH264VENC_ERR_PROCESS_CALL).

 

The error has been seen with encoder versions 2.20.00.005

and 2.30.00.01.

 

The error frequently occurs when the scene content changes from

complex moving objects to a blank single color.

 

The higher you set the bitrate, the more frequently the error occurs.

 

Can you confirm this issue?

My parameters are given below for 360x240 resolution  at 10Mbits/second,

it shows the issue frequently.

 

h264enc version 02.30.00.01

Base params
===========
size 124
encodingPreset        3
rateControlPreset     5
maxHeight             256
maxWidth              368
maxFrameRate          30000
dataEndianness        1
maxInterFrameInterval 0
inputChromaFormat     9
inputContentType      0
reconChromaFormat     9
profileIdc 100
levelIdc 30
Log2MaxFrameNumMinus4 0
ConstraintSetFlag 0
entropyMode 1
transform8x8FlagIntraFrame 0
transform8x8FlagInterFrame 0
enableVUIparams 7
meAlgo 1
seqScalingFlag 1
encQuality 0
enableARM926Tcm 0
enableDDRbuff 0
sliceMode 3
EnableLongTermFrame 0
outputDataMode 0
sliceFormat 1


==============
size                212
inputHeight         240
inputWidth          360
refFrameRate        30000
targetFrameRate     30000
targetBitRate       10000000
intraFrameInterval  60
generateHeader      0
captureWidth        384
forceFrame          -1
interFrameInterval  1
mbDataFlag          0
sliceSize 1
airRate 0
intraFrameQP 28
interPFrameQP 28
initQ 28
rcQMax 51
rcQMin 5
rcQMaxI 40
rcQMinI 0
rcAlgo 6
maxDelay 300
aspectRatioX 10
aspectRatioY 11
lfDisableIdc 0
enableBufSEI 1
enablePicTimSEI 0
perceptualRC 0
idrFrameInterval 60
mvSADoutFlag 0
resetHDVICPeveryFrame 0
enableROI 0
metaDataGenerateConsume 0
disableMVDCostFactor 0
putDataGetSpaceFxn 60664
interlaceRefMode 0
maxBitrateCVBR 10000000
enableGDR 0
GDRduration 0
GDRinterval 0
LongTermRefreshInterval 0
UseLongTermFrame 0
SetLongTermFrame 0
VUI_Buffer 1601672
aspectRatioInfoPresentFlag 1
overscanInfoPresentFlag 0
overscanAppropriateFlag 0
videoSignalTypePresentFlag 1
videoFormat 2
pixelRange 1
colourDescriptionPresentFlag 0
colourPrimaries 2
transferCharacteristics 2
matrixCoefficients 2
timingInfoPresentFlag 1
numUnitsInTicks 1001
timeScale 60000
fixedFrameRateFlag 1
nalHrdParameterspresentFlag 1
picStructPresentFlag 0
bitstreamRestrictionFlag 1
CustomScaleMatrix_Buffer 1577828
CVBRsensitivity 0
CVBRminbitrate 0
LBRmaxpicsize 76
LBRminpicsize 0
LBRskipcontrol 327684
dataSyncHandle 1591288
.
.
.
@0x004592b2:[T:0x42522490] ti.sdo.dmai - [Venc1] VIDENC1_process() failed with error (-1 ext: 0x8010)
Error: Failed to encode video buffer

 

 

Regards,

John Whittington