Dear TI staff,
We recently found that the imx219.ko built from processor sdk version 8.6 seems to have some problem: sometimes the imx219 camera failed to be probed, and in other cases the gstreamer pipeline utilizing imx219 would stuck after printing 'New clock: GstSystemClock'. On the contrary, when we use the imx219.ko from prebuilt image, everthing works fine.
We haven't modify anything in the driver code yet, so we want to ask if you could comfirm the availability of the code?
Another issue is about the patchwork mentioned in this link(https://software-dl.ti.com/jacinto7/esd/processor-sdk-linux-edgeai/AM62AX/08_06_00/exports/docs/devices/AM62AX/linux/getting_started.html#rpiv2-imx219-raw-sensor). It provides 1920x1080@60fps mode which we would like to try out, but it seems the patch is not for the current version of the driver code. If possible, would you also provide us with a feasible imx219 driver code that can produce 1920x1080@60fps stream?
Thank you for your support in advance.
Regards,
Huang Jingjie