7522.ezsdk_5_01_01_80_dm816x-c6a816x-am389x_Release_Notes(1).pdf
I am designing DM8168 target board.
Could you tell me the considerations of designing target board using EzSDK 5.01.01.80?
Attached release notes describes below.
(P.7) Known Issues and Limitations
Limitations
1. External video capture is only supported through the TVP7002 video decoder via I2C1.
Customers are required to maintain the same configuration on their boards. The EZSDK will
support additional capture devices in future releases.
Customers will also be able to add capture devices of their choice in future releases.
What is the meaning of "the same configuration"?
Is it OK if the same circuit design as EVM?
Are there other consideration rules?
3. The Media Controller HDVICP2 firmware initializes and configures the EIO (Expansion IO)
card. Existing Integra/Sitara customers with DDR2 or DDR3 boards and who do not have the
EIO card should not install the multimedia components.
I think should be same memory mapping for the HDVICP2 firmware.
Are there other consideration rules about hw design etc.. ?