Hi,
I have a custom made AM1808 board that works very fine, however it has two interesting problems, two GPIOs are not working, the GPIO numbers are:
GPIO6[13] (GPIO Pin 110, R17) and GPIO2[4] (GPIO Pin 37, A9)
I have verified that they are connected to the correct pins (according to AM1808 datasheet), however I cannot export them in Linux /sys/, all the pin mappings seem to be fine, that is I have defined the pins to be GPIOs. I have also verified that GPIO6[12], GPIO6[14] and GPIO2[3], GPIO2[5] works as expected and can be exported in /sys/.
What could be the reason for this behaviour?
Best Regards.
Niclas