This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Calculate bandwidth for DM365 system



Hello

I am working a DM365 video system. There are two imporatnt parts in my system and one is VPFE and the other is VFBE.

In VPFE module, the Dm365 will be connected with a CMOS sensor and sensor resolution is 1024*768 and frame rate is 60 fps at the same time.meanwhile,the sensor output is 10-bit.

In VPFE module, the DM365 will be connected with a LCD device. DM365 must be configured to provide VGA(640*480) output at 60fps.

And we want to use one DDR whose clock is 243Mhz in this DM365 system.

Could you tell me if the DM365 systen can meet  bandwidh?

I  do not know how to calculate.  I am very appreciate if you can give me some advice and calculation in details.

Maybe you can provide some conference about bandwidth calculation.

Thank you.