This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM623: SDK Linux v9 Building the SDK Fails

Part Number: AM623


Following the steps outlined here: https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/latest/exports/docs/linux/Overview_Building_the_SDK.html

The build ultimately fails because it cannot clone the submodules in .../tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/powervr-graphics/5.10-r0/git/

If I navigate to that directory and go a 'git submodule init' and 'git submodule update' manually and then re-run the bitbake command then all task complete successfully.

I have the proxies configured correctly to clone everything else in the build process successfully.

Error log here:

...

| Submodule glm not initalised, Attempting to fetch now

| Cloning into '/home/asdf/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/powervr-graphics/5.10-r0/git/external/glm/source'...

| fatal: unable to access 'https://github.com/g-truc/glm.git/': Could not resolve host: github.com

| fatal: clone of 'https://github.com/g-truc/glm.git' into submodule path '/home/asdf/tisdk/build/arago-tmp-default-glibc/work/aarch64-oe-linux/powervr-graphics/5.10-r0/git/external/glm/source' failed

| Failed to clone 'external/glm/source'. Retry scheduled