Part Number: TMDS64EVM
Dear Experts,
I have a custom sbl ospi linux project and I am having some problems with Udma in this project.
I want to use both ethernet and crypto device (SA2UL) and Ospi Flash in the same project.
However, syscfg shows that the maximum number of udma instances can be 2.
On my side, Sbl uses BCDMA_0 as default, Etherhent and Crypto uses PKTDMA_0.
Syscfg does not support 3 udma instances.
That's why I don't use them together in the project.
What do you advise me to do in this situation?
I would be very grateful if you could help me.
I especially wonder if a software solution can be provided
Best Regard,
Tuna Girisken
CCS Version: 12.4.0
SDK Version: 08.06.00.45
Board: Hs-Fs and Gp doesnt mater (I mean i have both of them)