Part Number: TDA4VH-Q1
Other Parts Discussed in Thread: TDA4VH
Hi experts,
I am currently using the TDA4VH development board with SDK 8.6. I used the switch mode in native driver for testing.
I have a question: When using the switch mode under the native driver, it is necessary to use it together with the bridge.
So, is the forwarding function performed by the CPSW hardware or by the software protocol stack in the bridge?
My understanding is that it directly forwards through MAC addresses in the switch hardware,
is that correct?
regards
yrq