Part Number: AM625
Other Parts Discussed in Thread: TLV320AIC26
We have a working boot using a AM6254 processors. Trying to bring up the AM6252 processors and I am seeing a remoteproc synchronous external abort kernel dump. My understanding is that the only difference with the 6252 is it has 2 ARM cores instead of 4 but this error seems to contradict that. Any idea whats going on?
[ 17.143823] k3-m4-rproc 5000000.m4fss: assigned reserved memory node m4f-dma-memory@9cb00000 [ 17.221196] k3-m4-rproc 5000000.m4fss: configured M4 for remoteproc mode [ 17.285665] k3-m4-rproc 5000000.m4fss: local reset is deasserted for device [ 17.364848] remoteproc remoteproc0: 5000000.m4fss is available [ 17.397859] remoteproc remoteproc0: powering up 5000000.m4fss [ 17.403712] remoteproc remoteproc0: Booting fw image am62-mcu-m4f0_0-fw, size 54860 [ 17.420106] remoteproc0#vdev0buffer: assigned reserved memory node m4f-dma-memory@9cb00000 [ 17.431819] virtio_rpmsg_bus virtio0: rpmsg host is online [ 17.443375] remoteproc0#vdev0buffer: registered virtio0 (type 7) [ 17.449523] remoteproc remoteproc0: remote processor 5000000.m4fss is now up [ 17.463138] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xd [ 17.471102] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xe [ 17.491528] Internal error: synchronous external abort: 96000010 [#1] PREEMPT SMP [ 17.499023] Modules linked in: dwc3_am62(+) rti_wdt(+) virtio_rpmsg_bus ti_k3_m4_remoteproc snd_soc_tlv320aic26 sa2ul pruss sha512_generic authenc cdns_dphy ltc2945 at24 sch_fq_codel cryptodev(O) ipv6 [ 17.516894] CPU: 1 PID: 219 Comm: systemd-udevd Tainted: G O 5.10.168-yocto-standard #1 [ 17.526191] Hardware name: Critical Link MitySOM-AM62x (DT) [ 17.531760] pstate: 80000005 (Nzcv daif -PAN -UAO -TCO BTYPE=--) [ 17.537772] pc : rti_wdt_probe+0x1e8/0x4f0 [rti_wdt] [ 17.542738] lr : rti_wdt_probe+0x1d8/0x4f0 [rti_wdt] [ 17.547693] sp : ffff800011c5b920 [ 17.550999] x29: ffff800011c5b920 x28: 0000000000000100 [ 17.556309] x27: ffff80001011c1a8 x26: 0000000000000003 [ 17.561615] x25: ffff800011603d98 x24: 000000000000004a [ 17.566923] x23: ffff00000467a920 x22: ffff000002423400 [ 17.572231] x21: ffff00000467a890 x20: ffff000002423410 [ 17.577539] x19: ffff00000467a880 x18: 0000000000000000 [ 17.582848] x17: 0000000000000000 x16: 0000000000000000 [ 17.588155] x15: 0000000000000000 x14: ffff000005c0d580 [ 17.593463] x13: 0000000000000000 x12: ffff8000117dd000 [ 17.598769] x11: ffff8000117d7000 x10: 0000000000001000 [ 17.604078] x9 : ffff80001075c0fc x8 : ffff8000114c2b7c [ 17.609389] x7 : 0000000000000041 x6 : 000000000000008b [ 17.614697] x5 : 000000000e021000 x4 : ffff000002423610 [ 17.620005] x3 : ffff000005e5cd00 x2 : 0000000000000000 [ 17.625312] x1 : ffff000005c0b900 x0 : ffff8000117d5090 [ 17.630620] Call trace: [ 17.633071] rti_wdt_probe+0x1e8/0x4f0 [rti_wdt] [ 17.637691] platform_drv_probe+0x5c/0xb0 [ 17.641695] really_probe+0xf4/0x408 [ 17.645266] driver_probe_device+0x60/0xc0 [ 17.649357] device_driver_attach+0x7c/0x88 [ 17.653533] __driver_attach+0x70/0x100 [ 17.657362] bus_for_each_dev+0x78/0xc8 [ 17.661192] driver_attach+0x2c/0x38 [ 17.664762] bus_add_driver+0x15c/0x210 [ 17.668592] driver_register+0x6c/0x128 [ 17.672423] __platform_driver_register+0x50/0x60 [ 17.677124] rti_wdt_driver_init+0x2c/0x1000 [rti_wdt] [ 17.682260] do_one_initcall+0x4c/0x2e0 [ 17.686094] do_init_module+0x50/0x210 [ 17.689838] load_module+0x20fc/0x27a8 [ 17.693580] __do_sys_finit_module+0xb8/0xf8 [ 17.697843] __arm64_sys_finit_module+0x28/0x38 [ 17.702370] el0_svc_common.constprop.0+0x80/0x1d0 [ 17.707154] do_el0_svc+0x2c/0xa8 [ 17.710465] el0_svc+0x20/0x30 [ 17.713515] el0_sync_handler+0xb0/0xb8 [ 17.717343] el0_sync+0x180/0x1c0 [ 17.720659] Code: f9000260 b140041f 54001128 91024000 (b9400000) [ 17.726748] ---[ end trace fbd7824ab88012ad ]--- [ 17.797896] platform 78000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1) [ 17.923128] platform 78000000.r5f: configured R5F for IPC-only mode [ 17.988926] platform 78000000.r5f: assigned reserved memory node r5f-dma-memory@9da00000