We have a custom board using a C6746 with SDRAM (no DDR). I have been able to run a small program (non BIOS) that just toggles an LED out of SDRAM. When I try to run a BIOS program from SDRAM using the same GEL file, it never gets to main(). When I halt it is in an out of range memory area. If I look at where c_int00 is supposed to be, there is a static pattern there that does not look like code. I do not get any errors during the load. Is there a way to load the program without running at all? I'd like to know whether it is loading incorrectly or getting corrupted after running. Is there something wrong with my setup files? I have been able to run this program on the LogicPD EVM using a different GEL, config, and platform file. Is there something else I need to alter?
I am using BIOS 5.41.10.36, CCS 4.2, and a Blackhawk 560M emulator.
Attached are the GEL file Platform.tci, and project .cfg file.
#define PLL0_BASE 0x01C11000 /*SYSTEM PLL BASE ADDRESS*/
#define PLL0_PID *(unsigned int*) (PLL0_BASE + 0x00) /*PID*/
#define PLL0_RSTYPE *(unsigned int*) (PLL0_BASE + 0xE4) /*Reset Type status Reg*/
#define PLL0_PLLCTL *(unsigned int*) (PLL0_BASE + 0x100) /*PLL Control Register*/
#define PLL0_OCSEL *(unsigned int*) (PLL0_BASE + 0x104) /*OBSCLK Select Register*/
#define PLL0_SECCTL *(unsigned int*) (PLL0_BASE + 0x108) /*PLL Secondary Control Register*/
#define PLL0_PLLM *(unsigned int*) (PLL0_BASE + 0x110) /*PLL Multiplier*/
#define PLL0_PREDIV *(unsigned int*) (PLL0_BASE + 0x114) /*Pre divider*/
#define PLL0_PLLDIV1 *(unsigned int*) (PLL0_BASE + 0x118) /*Divider-1*/
#define PLL0_PLLDIV2 *(unsigned int*) (PLL0_BASE + 0x11C) /*Divider-2*/
#define PLL0_PLLDIV3 *(unsigned int*) (PLL0_BASE + 0x120) /*Divider-3*/
#define PLL0_OSCDIV1 *(unsigned int*) (PLL0_BASE + 0x124) /*Oscilator Divider*/
#define PLL0_POSTDIV *(unsigned int*) (PLL0_BASE + 0x128) /*Post Divider*/
#define PLL0_BPDIV *(unsigned int*) (PLL0_BASE + 0x12C) /*Bypass Divider*/
#define PLL0_WAKEUP *(unsigned int*) (PLL0_BASE + 0x130) /*Wakeup Reg*/
#define PLL0_PLLCMD *(unsigned int*) (PLL0_BASE + 0x138) /*Command Reg*/
#define PLL0_PLLSTAT *(unsigned int*) (PLL0_BASE + 0x13C) /*Status Reg*/
#define PLL0_ALNCTL *(unsigned int*) (PLL0_BASE + 0x140) /*Clock Align Control Reg*/
#define PLL0_DCHANGE *(unsigned int*) (PLL0_BASE + 0x144) /*PLLDIV Ratio Chnage status*/
#define PLL0_CKEN *(unsigned int*) (PLL0_BASE + 0x148) /*Clock Enable Reg*/
#define PLL0_CKSTAT *(unsigned int*) (PLL0_BASE + 0x14C) /*Clock Status Reg*/
#define PLL0_SYSTAT *(unsigned int*) (PLL0_BASE + 0x150) /*Sysclk status reg*/
#define PLL0_PLLDIV4 *(unsigned int*) (PLL0_BASE + 0x160) /*Divider 4*/
#define PLL0_PLLDIV5 *(unsigned int*) (PLL0_BASE + 0x164) /*Divider 5*/
#define PLL0_PLLDIV6 *(unsigned int*) (PLL0_BASE + 0x168) /*Divider 6*/
#define PLL0_PLLDIV7 *(unsigned int*) (PLL0_BASE + 0x16C) /*Divider 7*/
#define PLL0_PLLDIV8 *(unsigned int*) (PLL0_BASE + 0x170) /*Divider 8*/
#define PLL0_PLLDIV9 *(unsigned int*) (PLL0_BASE + 0x174) /*Divider 9*/
#define PLL0_PLLDIV10 *(unsigned int*) (PLL0_BASE + 0x178) /*Divider 10*/
#define PLL0_PLLDIV11 *(unsigned int*) (PLL0_BASE + 0x17C) /*Divider 11*/
#define PLL0_PLLDIV12 *(unsigned int*) (PLL0_BASE + 0x180) /*Divider 12*/
#define PLL0_PLLDIV13 *(unsigned int*) (PLL0_BASE + 0x184) /*Divider 13*/
#define PLL0_PLLDIV14 *(unsigned int*) (PLL0_BASE + 0x188) /*Divider 14*/
#define PLL0_PLLDIV15 *(unsigned int*) (PLL0_BASE + 0x18C) /*Divider 15*/
#define PLL0_PLLDIV16 *(unsigned int*) (PLL0_BASE + 0x190) /*Divider 16*/
#define PLL1_BASE 0x01E1A000 /*SYSTEM PLL1 BASE ADDRESS*/
#define PLL1_PID *(unsigned int*) (PLL1_BASE + 0x00) /*PID*/
#define PLL1_RSTYPE *(unsigned int*) (PLL1_BASE + 0xE4) /*Reset Type status Reg*/
#define PLL1_PLLCTL *(unsigned int*) (PLL1_BASE + 0x100) /*PLL Control Register*/
#define PLL1_OCSEL *(unsigned int*) (PLL1_BASE + 0x104) /*OBSCLK Select Register*/
#define PLL1_SECCTL *(unsigned int*) (PLL1_BASE + 0x108) /*PLL Secondary Control Register*/
#define PLL1_PLLM *(unsigned int*) (PLL1_BASE + 0x110) /*PLL Multiplier*/
#define PLL1_PREDIV *(unsigned int*) (PLL1_BASE + 0x114) /*Pre divider*/
#define PLL1_PLLDIV1 *(unsigned int*) (PLL1_BASE + 0x118) /*Divider-1*/
#define PLL1_PLLDIV2 *(unsigned int*) (PLL1_BASE + 0x11C) /*Divider-2*/
#define PLL1_PLLDIV3 *(unsigned int*) (PLL1_BASE + 0x120) /*Divider-3*/
#define PLL1_OSCDIV1 *(unsigned int*) (PLL1_BASE + 0x124) /*Oscilator Divider*/
#define PLL1_POSTDIV *(unsigned int*) (PLL1_BASE + 0x128) /*Post Divider*/
#define PLL1_BPDIV *(unsigned int*) (PLL1_BASE + 0x12C) /*Bypass Divider*/
#define PLL1_WAKEUP *(unsigned int*) (PLL1_BASE + 0x130) /*Wakeup Reg*/
#define PLL1_PLLCMD *(unsigned int*) (PLL1_BASE + 0x138) /*Command Reg*/
#define PLL1_PLLSTAT *(unsigned int*) (PLL1_BASE + 0x13C) /*Status Reg*/
#define PLL1_ALNCTL *(unsigned int*) (PLL1_BASE + 0x140) /*Clock Align Control Reg*/
#define PLL1_DCHANGE *(unsigned int*) (PLL1_BASE + 0x144) /*PLLDIV Ratio Chnage status*/
#define PLL1_CKEN *(unsigned int*) (PLL1_BASE + 0x148) /*Clock Enable Reg*/
#define PLL1_CKSTAT *(unsigned int*) (PLL1_BASE + 0x14C) /*Clock Status Reg*/
#define PLL1_SYSTAT *(unsigned int*) (PLL1_BASE + 0x150) /*Sysclk status reg*/
#define PLL1_PLLDIV4 *(unsigned int*) (PLL1_BASE + 0x160) /*Divider 4*/
#define PLL1_PLLDIV5 *(unsigned int*) (PLL1_BASE + 0x164) /*Divider 5*/
#define PLL1_PLLDIV6 *(unsigned int*) (PLL1_BASE + 0x168) /*Divider 6*/
#define PLL1_PLLDIV7 *(unsigned int*) (PLL1_BASE + 0x16C) /*Divider 7*/
#define PLL1_PLLDIV8 *(unsigned int*) (PLL1_BASE + 0x170) /*Divider 8*/
#define PLL1_PLLDIV9 *(unsigned int*) (PLL1_BASE + 0x174) /*Divider 9*/
#define PLL1_PLLDIV10 *(unsigned int*) (PLL1_BASE + 0x178) /*Divider 10*/
#define PLL1_PLLDIV11 *(unsigned int*) (PLL1_BASE + 0x17C) /*Divider 11*/
#define PLL1_PLLDIV12 *(unsigned int*) (PLL1_BASE + 0x180) /*Divider 12*/
#define PLL1_PLLDIV13 *(unsigned int*) (PLL1_BASE + 0x184) /*Divider 13*/
#define PLL1_PLLDIV14 *(unsigned int*) (PLL1_BASE + 0x188) /*Divider 14*/
#define PLL1_PLLDIV15 *(unsigned int*) (PLL1_BASE + 0x18C) /*Divider 15*/
#define PLL1_PLLDIV16 *(unsigned int*) (PLL1_BASE + 0x190) /*Divider 16*/
/*PSC Module Related Registers*/
#define PSC0_BASE 0x01C10000
#define PSC1_BASE 0x01E27000
#define PSC0_MDCTL (PSC0_BASE+0xA00)
#define PSC0_MDSTAT (PSC0_BASE+0x800)
#define PSC0_PTCMD *(unsigned int*) (PSC0_BASE + 0x120)
#define PSC0_PTSTAT *(unsigned int*) (PSC0_BASE + 0x128)
#define PSC1_MDCTL (PSC1_BASE+0xA00)
#define PSC1_MDSTAT (PSC1_BASE+0x800)
#define PSC1_PTCMD *(unsigned int*) (PSC1_BASE + 0x120)
#define PSC1_PTSTAT *(unsigned int*) (PSC1_BASE + 0x128)
#define PSC_TIMEOUT 200 // This value can be optimized by the user
#define LPSC_EDMA_CC0 0
#define LPSC_EDMA_TC0 1
#define LPSC_EDMA_TC1 2
#define LPSC_EMIFA 3 /*PSC0*/
#define LPSC_SPI0 4 /*PSC0*/
#define LPSC_MMCSD0 5 /*PSC0*/
// LPSC #6 not used
// LPSC #7 not used
// LPSC #8 not used
#define LPSC_UART0 9 /*PSC0*/
#define LPSC_SCR0 10
#define LPSC_SCR1 11
#define LPSC_SCR2 12
// LPSC #13 not used
// LPSC #14 not used
#define LPSC_DSP 15 /*PSC0*/
#define LPSC_EDMA_CC1 0
#define LPSC_USB20 1 /*PSC1*/
#define LPSC_USB11 2 /*PSC1*/
#define LPSC_GPIO 3 /*PSC1*/
#define LPSC_UHPI 4 /*PSC1*/
#define LPSC_EMAC 5 /*PSC1*/
#define LPSC_DDR 6 /*PSC1*/
#define LPSC_MCASP0 7 /*PSC1*/
#define LPSC_SATA 8 /*PSC1*/
#define LPSC_VPIF 9 /*PSC1*/
#define LPSC_SPI1 10 /*PSC1*/
#define LPSC_I2C1 11 /*PSC1*/
#define LPSC_UART1 12 /*PSC1*/
#define LPSC_UART2 13 /*PSC1*/
#define LPSC_MCBSP0 14 /*PSC1*/
#define LPSC_MCBSP1 15 /*PSC1*/
#define LPSC_LCDC 16 /*PSC1*/
#define LPSC_EPWM 17 /*PSC1*/
#define LPSC_MMCSD1 18
#define LPSC_UPP 19
#define LPSC_ECAP 20
#define LPSC_EDMA_TC2 21
// LPSC #22-23 not used
#define LPSC_SCR_F0 24
#define LPSC_SCR_F1 25
#define LPSC_SCR_F2 26
#define LPSC_SCR_F6 27
#define LPSC_SCR_F7 28
#define LPSC_SCR_F8 29
#define LPSC_BR_F7 30
#define LPSC_SHARED_RAM 31
/*DDR MMR Declaration*/
#define VTPIO_CTL *(unsigned int*)(0x01E2C000) //VTPIO_CTL Register
#define DDR_SLEW *(unsigned int*)(0x01E2C004) //DDR_SLEW Register
#define EMIFDDR_SDRAM_CFG 0xB0000000
#define EMIFDDR_REVID *(unsigned int*)(EMIFDDR_SDRAM_CFG + 0x00) //EMIF Module ID and Revision Register
#define EMIFDDR_SDRSTAT *(unsigned int*)(EMIFDDR_SDRAM_CFG + 0x04) //SDRAM Status Register
#define EMIFDDR_SDCR *(unsigned int*)(EMIFDDR_SDRAM_CFG + 0x08) //SDRAM Bank Config Register
#define EMIFDDR_SDRCR *(unsigned int*)(EMIFDDR_SDRAM_CFG + 0x0C) //SDRAM Refresh Control Register
#define EMIFDDR_SDTIMR1 *(unsigned int*)(EMIFDDR_SDRAM_CFG + 0x10) //SDRAM Timing Register1
#define EMIFDDR_SDTIMR2 *(unsigned int*)(EMIFDDR_SDRAM_CFG + 0x14) //SDRAM Timing Register2
#define EMIFDDR_SDCR2 *(unsigned int*)(EMIFDDR_SDRAM_CFG + 0x1C) //SDRAM Config Register2
#define EMIFDDR_PBBPR *(unsigned int*)(EMIFDDR_SDRAM_CFG + 0x20) //VBUSM Burst Priority Register
#define EMIFDDR_VBUSMCFG1 *(unsigned int*)(EMIFDDR_SDRAM_CFG + 0x28) //VBUSM config Value1 Register
#define EMIFDDR_VBUSMCFG2 *(unsigned int*)(EMIFDDR_SDRAM_CFG + 0x2C) //VBUSM config Value2 Register
#define EMIFDDR_IRR *(unsigned int*)(EMIFDDR_SDRAM_CFG + 0xC0) //Interrupt Raw Register
#define EMIFDDR_IMR *(unsigned int*)(EMIFDDR_SDRAM_CFG + 0xC4) //Interrupt Masked Register
#define EMIFDDR_IMSR *(unsigned int*)(EMIFDDR_SDRAM_CFG + 0xC8) //Interrupt Mask Set Register
#define EMIFDDR_IMCR *(unsigned int*)(EMIFDDR_SDRAM_CFG + 0xCC) //Interrupt Mask Clear Register
#define DDRPHYREV *(unsigned int*)(EMIFDDR_SDRAM_CFG + 0xE0) //DDR PHY ID and Revision Register
#define DRPYC1R *(unsigned int*)(EMIFDDR_SDRAM_CFG + 0xE4) //DDR PHY Control 1 Register
#define DDR2 0 // Do not change this value
#define MDDR 1 // Do not change this value
#define VTP_TIMEOUT 200 // This value can be optimized by the user
#define DDR_DEBUG 0 // Set this to "1" to program DDR with more timing slack
#define EMIFDDR_BASE_ADDR 0xC0000000
#define EMIFA_BASE_ADDR 0x40000000
#define EMIFA_CS2_BASE_ADDR 0x60000000
#define EMIFA_CS3_BASE_ADDR 0x62000000
#define EMIFA_CS4_BASE_ADDR 0x64000000
#define EMIFA_CS5_BASE_ADDR 0x66000000
/*EMIF2.5 MMR Declaration*/
#define EMIFA 0x68000000
#define EMIFA_AWAITCFG *(unsigned int*)(EMIFA + 0x04)
#define EMIFA_SDCFG *(unsigned int*)(EMIFA + 0x08)
#define EMIFA_SDREF *(unsigned int*)(EMIFA + 0x0C)
#define EMIFA_ACFG2 *(unsigned int*)(EMIFA + 0x10) //Async Bank1 Config Register
#define EMIFA_ACFG3 *(unsigned int*)(EMIFA + 0x14) //Async Bank2 Config Register
#define EMIFA_ACFG4 *(unsigned int*)(EMIFA + 0x18) //Async Bank3 Config Register
#define EMIFA_ACFG5 *(unsigned int*)(EMIFA + 0x1C) //Async Bank4 Config Register
#define EMIFA_SDTIM *(unsigned int*)(EMIFA + 0x20) //SDRAM Timing Register
#define EMIFA_SRPD *(unsigned int*)(EMIFA + 0x3C)
#define EMIFA_NANDFCR *(unsigned int*)(EMIFA + 0x60)
#define EMIFA_SDCR *(unsigned int*)(EMIFA + 0x08)
#define EMIFA_SDCR_MSB *(unsigned char*)(EMIFA + 0x0A)
#define EMIFA_SDTMR *(unsigned int*)(EMIFA + 0x20)
#define EMIFA_SDSRETR *(unsigned int*)(EMIFA + 0x3C)
#define EMIFA_SDRCR *(unsigned int*)(EMIFA + 0x0C)
#define RAM_BASE *(unsigned int*)(0x40000000)
/*GPIO MMR*/
#define GPIO_REG_BASE (0x01E26000)
#define GPIO_BANK_OFFSET (0x28)
#define GPIO_DAT_OFFSET (0x04)
#define GPIO_SET_OFFSET (0x08)
#define GPIO_CLR_OFFSET (0x0C)
#define GPIO_BINTEN *(unsigned int*)(GPIO_REG_BASE + 0x08)
#define GPIO_BANK01_BASE (GPIO_REG_BASE + 0x10)
#define GPIO_BANK23_BASE (GPIO_BANK01_BASE + GPIO_BANK_OFFSET)
#define GPIO_BANK45_BASE (GPIO_BANK23_BASE + GPIO_BANK_OFFSET)
#define GPIO_BANK67_BASE (GPIO_BANK45_BASE + GPIO_BANK_OFFSET)
#define GPIO_BANK8_BASE (GPIO_BANK67_BASE + GPIO_BANK_OFFSET)
#define GPIO_BANK23_DIR *(unsigned int*)(GPIO_BANK23_BASE)
#define GPIO_BANK23_DAT *(unsigned int*)(GPIO_BANK23_BASE + GPIO_DAT_OFFSET)
#define GPIO_BANK23_SET *(unsigned int*)(GPIO_BANK23_BASE + GPIO_SET_OFFSET)
#define GPIO_BANK23_CLR *(unsigned int*)(GPIO_BANK23_BASE + GPIO_CLR_OFFSET)
/*System MMR Declaration*/
#define SYS_BASE 0x01C14000
#define KICK0R *(unsigned int*)(SYS_BASE + 0x038)
#define KICK1R *(unsigned int*)(SYS_BASE + 0x03c)
#define PINMUX0 *(unsigned int*)(SYS_BASE + 0x120) //PINMUX0
#define PINMUX1 *(unsigned int*)(SYS_BASE + 0x124) //PINMUX1
#define PINMUX2 *(unsigned int*)(SYS_BASE + 0x128) //PINMUX2
#define PINMUX3 *(unsigned int*)(SYS_BASE + 0x12C) //PINMUX3
#define PINMUX4 *(unsigned int*)(SYS_BASE + 0x130) //PINMUX4
#define PINMUX5 *(unsigned int*)(SYS_BASE + 0x134) //PINMUX5
#define PINMUX6 *(unsigned int*)(SYS_BASE + 0x138) //PINMUX6
#define PINMUX7 *(unsigned int*)(SYS_BASE + 0x13C) //PINMUX7
#define PINMUX8 *(unsigned int*)(SYS_BASE + 0x140) //PINMUX8
#define PINMUX9 *(unsigned int*)(SYS_BASE + 0x144) //PINMUX9
#define PINMUX10 *(unsigned int*)(SYS_BASE + 0x148) //PINMUX10
#define PINMUX11 *(unsigned int*)(SYS_BASE + 0x14C) //PINMUX11
#define PINMUX12 *(unsigned int*)(SYS_BASE + 0x150) //PINMUX12
#define PINMUX13 *(unsigned int*)(SYS_BASE + 0x154) //PINMUX13
#define PINMUX14 *(unsigned int*)(SYS_BASE + 0x158) //PINMUX14
#define PINMUX15 *(unsigned int*)(SYS_BASE + 0x15C) //PINMUX15
#define PINMUX16 *(unsigned int*)(SYS_BASE + 0x160) //PINMUX16
#define PINMUX17 *(unsigned int*)(SYS_BASE + 0x164) //PINMUX17
#define PINMUX18 *(unsigned int*)(SYS_BASE + 0x168) //PINMUX18
#define PINMUX19 *(unsigned int*)(SYS_BASE + 0x16C) //PINMUX19
#define CFGCHIP0 *(unsigned int*)(SYS_BASE + 0x17C)
#define CFGCHIP2 *(unsigned int*)(SYS_BASE + 0x184)
#define CFGCHIP3 *(unsigned int*)(SYS_BASE + 0x188)
#define PD0 0 /*Power Domain-0*/
#define PD1 1 /*Power Domain-1*/
#define PLLEN_MUX_SWITCH 4
#define PLL_LOCK_TIME_CNT 2400
#define PLL_STABILIZATION_TIME 2000
#define PLL_RESET_TIME_CNT 200
OnTargetConnect( )
{
GEL_TextOut("\tTarget Connected.\n","Output",1,1,1);
GEL_TextOut("\t---------------------------------------------\n","Output",1,1,1);
Clear_Memory_Map();
Setup_Memory_Map();
DEVICE_kickUnlock(); // No longer needed for Si Rev 2.0+
//PSC_All_On_Full_EVM();
//Core_300MHz_mDDR_150MHz();
Set_Core_300MHz();
Set_SDRAM();
}
menuitem "OMAP-L138 Memory Map"
/* ------------------------------------------------------------------------ *
* *
* Clear_Memory_Map( ) *
* Clear the Memory Map *
* *
* ------------------------------------------------------------------------ */
hotmenu Clear_Memory_Map()
{
GEL_MapOff( );
GEL_MapReset( );
GEL_TextOut("\tMemory Map Cleared.\n","Output",1,1,1);
GEL_TextOut("\t---------------------------------------------\n","Output",1,1,1);
}
hotmenu Setup_Memory_Map()
{
GEL_MapOn( );
GEL_MapReset( );
/* DSP */
GEL_MapAddStr( 0x00700000, 0, 0x00100000, "R|W|AS4", 0 ); // DSP L2 ROM
GEL_MapAddStr( 0x00800000, 0, 0x00040000, "R|W|AS4", 0 ); // DSP l2 RAM
GEL_MapAddStr( 0x00E00000, 0, 0x00008000, "R|W|AS4", 0 ); // DSP L1P RAM
GEL_MapAddStr( 0x00F00000, 0, 0x00008000, "R|W|AS4", 0 ); // DSP L1D RAM
GEL_MapAddStr( 0x01800000, 0, 0x00010000, "R|W|AS4", 0 ); // DSP Interrupt Controller
GEL_MapAddStr( 0x01810000, 0, 0x00001000, "R|W|AS4", 0 ); // DSP Powerdown Controller
GEL_MapAddStr( 0x01811000, 0, 0x00001000, "R|W|AS4", 0 ); // DSP Security ID
GEL_MapAddStr( 0x01812000, 0, 0x00008000, "R|W|AS4", 0 ); // DSP Revision ID
GEL_MapAddStr( 0x01820000, 0, 0x00010000, "R|W|AS4", 0 ); // DSP EMC
GEL_MapAddStr( 0x01830000, 0, 0x00010000, "R|W|AS4", 0 ); // DSP Internal Reserved
GEL_MapAddStr( 0x01840000, 0, 0x00010000, "R|W|AS4", 0 ); // DSP Memory System
GEL_MapAddStr( 0x11700000, 0, 0x00100000, "R|W|AS4", 0 ); // DSP L2 ROM (mirror)
GEL_MapAddStr( 0x11800000, 0, 0x00040000, "R|W|AS4", 0 ); // DSP l2 RAM (mirror)
GEL_MapAddStr( 0x11E00000, 0, 0x00008000, "R|W|AS4", 0 ); // DSP L1P RAM (mirror)
GEL_MapAddStr( 0x11F00000, 0, 0x00008000, "R|W|AS4", 0 ); // DSP L1D RAM (mirror)
/* Shared RAM */
GEL_MapAddStr( 0x80000000, 0, 0x00020000, "R|W|AS4", 0 ); // Shared RAM
/* EMIFA */
// GEL_MapAddStr( 0x40000000, 0, 0x20000000, "R|W|AS4", 0 ); // EMIFA SDRAM Data
GEL_MapAddStr( 0x40000000, 0, 0x02000000, "R|W|AS4", 0 ); // EMIFA SDRAM Data
GEL_MapAddStr( 0x60000000, 0, 0x02000000, "R|W|AS4", 0 ); // EMIFA CS2
// GEL_MapAddStr( 0x62000000, 0, 0x02000000, "R|W|AS4", 0 ); // EMIFA CS3
// GEL_MapAddStr( 0x64000000, 0, 0x02000000, "R|W|AS4", 0 ); // EMIFA CS4
// GEL_MapAddStr( 0x66000000, 0, 0x02000000, "R|W|AS4", 0 ); // EMIFA CS5
GEL_MapAddStr( 0x68000000, 0, 0x00008000, "R|W|AS4", 0 ); // EMIFA Control
/* DDR */
// GEL_MapAddStr( 0xB0000000, 0, 0x00008000, "R|W|AS4", 0 ); // DDR Control
// GEL_MapAddStr( 0xC0000000, 0, 0x20000000, "R|W|AS4", 0 ); // DDR Data
/* Peripherals */
GEL_MapAddStr( 0x01C00000, 0, 0x00008000, "R|W|AS4", 0 ); // TPCC0
GEL_MapAddStr( 0x01C08000, 0, 0x00000400, "R|W|AS4", 0 ); // TPTC0
GEL_MapAddStr( 0x01C08400, 0, 0x00000400, "R|W|AS4", 0 ); // TPTC1
GEL_MapAddStr( 0x01C10000, 0, 0x00001000, "R|W|AS4", 0 ); // PSC 0
GEL_MapAddStr( 0x01C11000, 0, 0x00001000, "R|W|AS4", 0 ); // PLL Controller 0
GEL_MapAddStr( 0x01C12000, 0, 0x00001000, "R|W|AS4", 0 ); // Key Manager
GEL_MapAddStr( 0x01C13000, 0, 0x00001000, "R|W|AS4", 0 ); // SecCo
GEL_MapAddStr( 0x01C14000, 0, 0x00001000, "R|W|AS4", 0 ); // SysConfig
GEL_MapAddStr( 0x01C16000, 0, 0x00001000, "R|W|AS4", 0 ); // IOPU 0
GEL_MapAddStr( 0x01C17000, 0, 0x00001000, "R|W|AS4", 0 ); // IOPU 2
GEL_MapAddStr( 0x01C20000, 0, 0x00001000, "R|W|AS4", 0 ); // Timer64P 0
GEL_MapAddStr( 0x01C21000, 0, 0x00001000, "R|W|AS4", 0 ); // Timer64P 1
GEL_MapAddStr( 0x01C22000, 0, 0x00001000, "R|W|AS4", 0 ); // I2C 0
GEL_MapAddStr( 0x01C23000, 0, 0x00001000, "R|W|AS4", 0 ); // RTC
GEL_MapAddStr( 0x01C24000, 0, 0x00001000, "R|W|AS4", 0 ); // IOPU 1
GEL_MapAddStr( 0x01C30000, 0, 0x00000200, "R|W|AS4", 0 ); // PRU Data RAM 0
GEL_MapAddStr( 0x01C32000, 0, 0x00000200, "R|W|AS4", 0 ); // PRU Data RAM 1
GEL_MapAddStr( 0x01C34000, 0, 0x00004000, "R|W|AS4", 0 ); // PRU Control Registers
GEL_MapAddStr( 0x01C38000, 0, 0x00001000, "R|W|AS4", 0 ); // PRU 0 Config Memory
GEL_MapAddStr( 0x01C3C000, 0, 0x00001000, "R|W|AS4", 0 ); // PRU 1 Config Memory
GEL_MapAddStr( 0x01C40000, 0, 0x00001000, "R|W|AS4", 0 ); // MMC/SD 0
GEL_MapAddStr( 0x01C41000, 0, 0x00001000, "R|W|AS4", 0 ); // SPI 0
GEL_MapAddStr( 0x01C42000, 0, 0x00001000, "R|W|AS4", 0 ); // UART 0
GEL_MapAddStr( 0x01C43000, 0, 0x00001000, "R|W|AS4", 0 ); // MPU 0
GEL_MapAddStr( 0x01D00000, 0, 0x00001000, "R|W|AS4", 0 ); // McASP 0 Control
GEL_MapAddStr( 0x01D01000, 0, 0x00001000, "R|W|AS4", 0 ); // McASP 0 FIFO Ctrl
GEL_MapAddStr( 0x01D02000, 0, 0x00001000, "R|W|AS4", 0 ); // McASP 0 Data
GEL_MapAddStr( 0x01D0C000, 0, 0x00001000, "R|W|AS4", 0 ); // UART 1
GEL_MapAddStr( 0x01D0D000, 0, 0x00001000, "R|W|AS4", 0 ); // UART 2
GEL_MapAddStr( 0x01D0E000, 0, 0x00001000, "R|W|AS4", 0 ); // IOPU 4
GEL_MapAddStr( 0x01D10000, 0, 0x00000800, "R|W|AS4", 0 ); // McBSP 0 Control
GEL_MapAddStr( 0x01D10800, 0, 0x00000200, "R|W|AS4", 0 ); // McBSP 0 FIFO Ctrl
GEL_MapAddStr( 0x01D11000, 0, 0x00000800, "R|W|AS4", 0 ); // McBSP 1 Control
GEL_MapAddStr( 0x01D11800, 0, 0x00000200, "R|W|AS4", 0 ); // McBSP 1 FIFO Ctrl
GEL_MapAddStr( 0x01E00000, 0, 0x00010000, "R|W|AS4", 0 ); // USB0 (USB HS) Cfg
GEL_MapAddStr( 0x01E10000, 0, 0x00001000, "R|W|AS4", 0 ); // UHPI Cfg
GEL_MapAddStr( 0x01E11000, 0, 0x00001000, "R|W|AS4", 0 ); // UHPI (IODFT)
GEL_MapAddStr( 0x01E13000, 0, 0x00001000, "R|W|AS4", 0 ); // LCD Controller
GEL_MapAddStr( 0x01E14000, 0, 0x00001000, "R|W|AS4", 0 ); // MPU 1
GEL_MapAddStr( 0x01E15000, 0, 0x00001000, "R|W|AS4", 0 ); // MPU 2
GEL_MapAddStr( 0x01E16000, 0, 0x00001000, "R|W|AS4", 0 ); // UPP
GEL_MapAddStr( 0x01E17000, 0, 0x00001000, "R|W|AS4", 0 ); // VPIF
GEL_MapAddStr( 0x01E18000, 0, 0x00002000, "R|W|AS4", 0 ); // SATA
GEL_MapAddStr( 0x01E1A000, 0, 0x00001000, "R|W|AS4", 0 ); // PLL Controller 1
GEL_MapAddStr( 0x01E1B000, 0, 0x00001000, "R|W|AS4", 0 ); // MMC/SD 1
GEL_MapAddStr( 0x01E20000, 0, 0x00002000, "R|W|AS4", 0 ); // EMAC CPPI
GEL_MapAddStr( 0x01E22000, 0, 0x00001000, "R|W|AS4", 0 ); // EMAC CONTROL registers
GEL_MapAddStr( 0x01E23000, 0, 0x00001000, "R|W|AS4", 0 ); // EMAC registers
GEL_MapAddStr( 0x01E24000, 0, 0x00001000, "R|W|AS4", 0 ); // EMAC MDIO port
GEL_MapAddStr( 0x01E25000, 0, 0x00001000, "R|W|AS4", 0 ); // USB1 (USB FS)
GEL_MapAddStr( 0x01E26000, 0, 0x00001000, "R|W|AS4", 0 ); // GPIO
GEL_MapAddStr( 0x01E27000, 0, 0x00001000, "R|W|AS4", 0 ); // PSC 1
GEL_MapAddStr( 0x01E28000, 0, 0x00001000, "R|W|AS4", 0 ); // I2C 1
GEL_MapAddStr( 0x01E29000, 0, 0x00001000, "R|W|AS4", 0 ); // IOPU 3
GEL_MapAddStr( 0x01E2A000, 0, 0x00001000, "R|W|AS4", 0 ); // PBIST Controller
GEL_MapAddStr( 0x01E2B000, 0, 0x00001000, "R|W|AS4", 0 ); // PBIST Combiner
GEL_MapAddStr( 0x01E2C000, 0, 0x00001000, "R|W|AS4", 0 ); // System Config
GEL_MapAddStr( 0x01E30000, 0, 0x00008000, "R|W|AS4", 0 ); // TPCC1
GEL_MapAddStr( 0x01E38000, 0, 0x00000400, "R|W|AS4", 0 ); // TPTC2
GEL_MapAddStr( 0x01F00000, 0, 0x00001000, "R|W|AS4", 0 ); // EPWM 0
GEL_MapAddStr( 0x01F01000, 0, 0x00001000, "R|W|AS4", 0 ); // HRPWM 0
GEL_MapAddStr( 0x01F02000, 0, 0x00001000, "R|W|AS4", 0 ); // EPWM 1
GEL_MapAddStr( 0x01F03000, 0, 0x00001000, "R|W|AS4", 0 ); // HRPWM 1
GEL_MapAddStr( 0x01F06000, 0, 0x00001000, "R|W|AS4", 0 ); // ECAP 0
GEL_MapAddStr( 0x01F07000, 0, 0x00001000, "R|W|AS4", 0 ); // ECAP 1
GEL_MapAddStr( 0x01F08000, 0, 0x00001000, "R|W|AS4", 0 ); // ECAP 2
GEL_MapAddStr( 0x01F0B000, 0, 0x00001000, "R|W|AS4", 0 ); // IOPU 5
GEL_MapAddStr( 0x01F0C000, 0, 0x00001000, "R|W|AS4", 0 ); // Timer64P 2
GEL_MapAddStr( 0x01F0D000, 0, 0x00001000, "R|W|AS4", 0 ); // Timer64P 3
GEL_MapAddStr( 0x01F0E000, 0, 0x00001000, "R|W|AS4", 0 ); // SPI1
GEL_MapAddStr( 0x01F10000, 0, 0x00001000, "R|W|AS4", 0 ); // McBSP 0 FIFO Data
GEL_MapAddStr( 0x01F11000, 0, 0x00001000, "R|W|AS4", 0 ); // McBSP 1 FIFO Data
GEL_TextOut("\tMemory Map Setup Complete.\n","Output",1,1,1);
GEL_TextOut("\t---------------------------------------------\n","Output",1,1,1);
}
hotmenu EMIFA_PINMUX()
{
PSC0_LPSC_enable(0, LPSC_EMIFA);
PINMUX5 = (PINMUX5 & ~0xFF000000) | 0x11000000;
PINMUX6 = 0x11111111;
PINMUX7 = 0x11111111;
PINMUX8 = 0x11111111;
PINMUX9 = 0x11111111;
PINMUX10 = 0x11111111;
PINMUX11 = 0x11111111;
PINMUX12 = 0x11111111;
GEL_TextOut("\tEMIFA Pins Configured.\n","Output",1,1,1);
GEL_TextOut("\t---------------------------------------------\n","Output",1,1,1);
}
Set_SDRAM()
{
int ramRead;
EMIFA_PINMUX();
EMIFA_SDTMR = 0x29114510;
// EMIFA_SDTMR = 0x29124510;
EMIFA_SDSRETR = 0x00000006;
// EMIFA_SDRCR = 0x0000030E;
EMIFA_SDRCR = 0x000009C5; // > 200 usec
// EMIFA_SDCR = 0x00004421;
EMIFA_SDCR = 0x00004521;
// Wait 200 usec
ramRead = RAM_BASE;
// update SDRCR
EMIFA_SDRCR = 0x0000030E;
}
Set_Core_300MHz()
{
// EMIFA_SDCR_MSB |= 0x80; // Set Self Refresh bit before configuring PLL0
device_PLL0(0, // 0: on chip osc, 1: ext osc
23, // PLLM: mulitplier - 1
1, // PostDiv: ratio - 1
0, // Div1: ratio - 1
1, // Div2: ratio - 1
2, // Div3: ratio - 1
5); // Div7: ratio - 1
// EMIFA_SDCR_MSB &= ~0x80; // Exit Self Refresh mode
GEL_TextOut("\tPLL0 init done for Core:300MHz, EMIFA:100MHz\n","Output",1,1,1);
}
/**************************************************************************************************************************************************
Device_PLL0 init:
CLKMODE - 0---->On Chip Oscilator 1---->External Oscilator
PLL0_SYSCLK1 - Fixed ratio /1
PLL0_SYSCLK2 - Fixed ratio /2
PLL0_SYSCLK3 - Variable Divider (EMIFA)
PLL0_SYSCLK4 - Fixed ratio /4
PLL0_SYSCLK5 - Not used -- do nothing
PLL0_SYSCLK6 - Fixed ratio /1
PLL0_SYSCLK7 - Variable Divider (RMII)
******************************************************************************************************************************************************/
device_PLL0(unsigned int CLKMODE, unsigned int PLLM, unsigned int POSTDIV,unsigned int PLLDIV1, unsigned int PLLDIV2, unsigned int PLLDIV3, unsigned int PLLDIV7 ) {
unsigned int i=0;
/* Clear PLL lock bit */
CFGCHIP0 &= ~(0x00000010);
/* Set PLLENSRC '0',bit 5, PLL Enable(PLLEN) selection is controlled through MMR */
PLL0_PLLCTL &= ~(0x00000020);
/* PLLCTL.EXTCLKSRC bit 9 should be left at 0 for Freon */
PLL0_PLLCTL &= ~(0x00000200);
/* Set PLLEN=0 to put in bypass mode*/
PLL0_PLLCTL &= ~(0x00000001);
/*wait for 4 cycles to allow PLLEN mux switches properly to bypass clock*/
for(i=0; i<PLLEN_MUX_SWITCH; i++) {;}
/* Select the Clock Mode bit 8 as External Clock or On Chip Oscilator*/
PLL0_PLLCTL &= 0xFFFFFEFF;
PLL0_PLLCTL |= (CLKMODE << 8);
/*Clear PLLRST bit to reset the PLL */
PLL0_PLLCTL &= ~(0x00000008);
/* Disable the PLL output*/
PLL0_PLLCTL |= (0x00000010);
/* PLL initialization sequence
Power up the PLL by setting PWRDN bit set to 0 */
PLL0_PLLCTL &= ~(0x00000002);
/* Enable the PLL output*/
PLL0_PLLCTL &= ~(0x00000010);
/*PLL stabilisation time- take out this step , not required here when PLL in bypassmode*/
for(i=0; i<PLL_STABILIZATION_TIME; i++) {;}
/*Program the required multiplier value in PLLM*/
PLL0_PLLM = PLLM;
/*If desired to scale all the SYSCLK frequencies of a given PLLC, program the POSTDIV ratio*/
PLL0_POSTDIV = 0x8000 | POSTDIV;
/*Check for the GOSTAT bit in PLLSTAT to clear to 0 to indicate that no GO operation is currently in progress*/
while(PLL0_PLLSTAT & 0x1==1){}
/*Program the RATIO field in PLLDIVx with the desired divide factors. In addition, make sure in this step you leave the PLLDIVx.DxEN bits set so clocks are still enabled (default).*/
PLL0_PLLDIV1 = 0x8000 | PLLDIV1; // Fixed Ratio /1
PLL0_PLLDIV2 = 0x8000 | PLLDIV2; // Fixed Ratio /2
PLL0_PLLDIV4 = 0x8000 | (((PLLDIV1+1)*4)-1); // Fixed Ratio /4
PLL0_PLLDIV6 = 0x8000 | PLLDIV1; // Fixed Ratio /1
PLL0_PLLDIV3 = 0x8000 | PLLDIV3; // Variable Ratio (EMIF)
PLL0_PLLDIV7 = 0x8000 | PLLDIV7; // Variable Ratio (RMII)
/*Set the GOSET bit in PLLCMD to 1 to initiate a new divider transition.*/
PLL0_PLLCMD |= 0x1;
/*Wait for the GOSTAT bit in PLLSTAT to clear to 0 (completion of phase alignment).*/
while(PLL0_PLLSTAT & 0x1==1) { }
/*Wait for PLL to reset properly.*/
for(i=0; i<PLL_RESET_TIME_CNT; i++) {;}
/*Set the PLLRST bit in PLLCTL to 1 to bring the PLL out of reset*/
PLL0_PLLCTL |= 0x8;
/*Wait for PLL to lock.*/
for(i=0; i<PLL_LOCK_TIME_CNT; i++) {;}
/*Set the PLLEN bit in PLLCTL to 1 to remove the PLL from bypass mode*/
PLL0_PLLCTL |= 0x1;
}
/**********************************************************************************
DDR PLL1 init:
***********************************************************************************/
device_PLL1(unsigned int PLLM,unsigned int POSTDIV,unsigned int PLLDIV1, unsigned int PLLDIV2, unsigned int PLLDIV3 ) {
unsigned int i=0;
/* Clear PLL lock bit */
CFGCHIP3 &= ~(0x00000020);
/* Set PLLENSRC '0',bit 5, PLL Enable(PLLEN) selection is controlled through MMR */
PLL1_PLLCTL &= ~(0x00000020);
/* PLLCTL.EXTCLKSRC bit 9 should be left at 0 for Freon */
PLL1_PLLCTL &= ~(0x00000200);
/* Set PLLEN=0 to put in bypass mode*/
PLL1_PLLCTL &= ~(0x00000001);
/*wait for 4 cycles to allow PLLEN mux switches properly to bypass clock*/
for(i=0; i<PLLEN_MUX_SWITCH; i++) {;}
/*Clear PLLRST bit to reset the PLL */
PLL1_PLLCTL &= ~(0x00000008);
/* Disable the PLL output*/
PLL1_PLLCTL |= (0x00000010);
/* PLL initialization sequence
Power up the PLL by setting PWRDN bit set to 0 */
PLL1_PLLCTL &= ~(0x00000002);
/* Enable the PLL output*/
PLL1_PLLCTL &= ~(0x00000010);
/*PLL stabilisation time- take out this step , not required here when PLL in bypassmode*/
for(i=0; i<PLL_STABILIZATION_TIME; i++) {;}
/*Program the required multiplier value in PLLM*/
PLL1_PLLM = PLLM;
/*If desired to scale all the SYSCLK frequencies of a given PLLC, program the POSTDIV ratio*/
PLL1_POSTDIV = 0x8000 | POSTDIV;
/*Check for the GOSTAT bit in PLLSTAT to clear to 0 to indicate that no GO operation is currently in progress*/
while(PLL1_PLLSTAT & 0x1==1){}
/*Program the RATIO field in PLLDIVx with the desired divide factors. In addition, make sure in this step you leave the PLLDIVx.DxEN bits set so clocks are still enabled (default).*/
PLL1_PLLDIV1 = 0x8000 | PLLDIV1; // DDR frequency (aka 2X_CLK)
PLL1_PLLDIV2 = 0x8000 | PLLDIV2; // Optional CFGCHIP3[ASYNC3_CLKSRC] clock source
PLL1_PLLDIV3 = 0x8000 | PLLDIV3; // Optional PLL0 clock source
/*Set the GOSET bit in PLLCMD to 1 to initiate a new divider transition.*/
PLL1_PLLCMD |= 0x1;
/*Wait for the GOSTAT bit in PLLSTAT to clear to 0 (completion of phase alignment).*/
while(PLL1_PLLSTAT & 0x1==1) { }
/*Wait for PLL to reset properly */
for(i=0; i<PLL_RESET_TIME_CNT; i++) {;}
/*Set the PLLRST bit in PLLCTL to 1 to bring the PLL out of reset*/
PLL1_PLLCTL |= 0x8;
/*Wait for PLL to lock. See PLL spec for PLL lock time*/
for(i=0; i<PLL_LOCK_TIME_CNT; i++) {;}
/*Set the PLLEN bit in PLLCTL to 1 to remove the PLL from bypass mode*/
PLL1_PLLCTL |= 0x1;
}
/**********************************************************************************
Device Kick Unlock:
Kick0 register + data (unlock)
Kick1 register + data (unlock)
***********************************************************************************/
DEVICE_kickUnlock() {
KICK0R = 0x83e70b13; // Kick0 register + data (unlock)
KICK1R = 0x95a4f1e0; // Kick1 register + data (unlock)
GEL_TextOut("\tKICK Unlocked.\n","Output",1,1,1);
GEL_TextOut("\t---------------------------------------------\n","Output",1,1,1);
}
/**********************************************************************************
PSC Common functions :
***********************************************************************************/
/*Force module state without handshaking */
PSC1_LPSC_force(unsigned int LPSC_num) {
*(unsigned int*) (PSC1_MDCTL+4*LPSC_num) = (*(unsigned int*) (PSC1_MDCTL+4*LPSC_num) | 0x80000000);
}
/*SyncReset Function for PSC1*/
PSC1_LPSC_SyncReset(unsigned int PD, unsigned int LPSC_num) {
unsigned int j;
if( (*(unsigned int*)(PSC1_MDSTAT+4 * LPSC_num) & 0x1F) != 0x1 ) {
*(unsigned int*) (PSC1_MDCTL+4*LPSC_num) = (*(unsigned int*) (PSC1_MDCTL+4*LPSC_num) & 0xFFFFFFE0) | 0x0001;
PSC1_PTCMD = 0x1<<PD;
j = 0;
/*Wait for power state transition to finish*/
while( (PSC1_PTSTAT & (0x1<<PD) ) !=0) {
if( j++ > PSC_TIMEOUT ) {
GEL_TextOut("\tPSC1 Sync Reset Transition Timeout on Domain %d, LPSC %d\n","Output",1,1,1,PD,LPSC_num);
break;
}
}
j = 0;
while( (*(unsigned int*)(PSC1_MDSTAT+4 * LPSC_num) & 0x1F) !=0x1) {
if( j++ > PSC_TIMEOUT ) {
GEL_TextOut("\tPSC1 Sync Reset Verify Timeout on Domain %d, LPSC %d\n","Output",1,1,1,PD,LPSC_num);
break;
}
}
}
}
/*Enable Function for PSC1*/
PSC1_LPSC_enable(unsigned int PD, unsigned int LPSC_num) {
unsigned int j;
if( (*(unsigned int*)(PSC1_MDSTAT+4 * LPSC_num) & 0x1F) != 0x3 ) {
*(unsigned int*) (PSC1_MDCTL+4*LPSC_num) = (*(unsigned int*) (PSC1_MDCTL+4*LPSC_num) & 0xFFFFFFE0) | 0x0003;
PSC1_PTCMD = 0x1<<PD;
j = 0;
/*Wait for power state transition to finish*/
while( (PSC1_PTSTAT & (0x1<<PD) ) !=0) {
if( j++ > PSC_TIMEOUT ) {
GEL_TextOut("\tPSC1 Enable Transition Timeout on Domain %d, LPSC %d\n","Output",1,1,1,PD,LPSC_num);
break;
}
}
j = 0;
while( (*(unsigned int*)(PSC1_MDSTAT+4 * LPSC_num) & 0x1F) !=0x3) {
if( j++ > PSC_TIMEOUT ) {
GEL_TextOut("\tPSC1 Enable Verify Timeout on Domain %d, LPSC %d\n","Output",1,1,1,PD,LPSC_num);
break;
}
}
}
}
/*LPSC Enable Function for DSP*/
PSC0_LPSC_enableCore(unsigned int PD, unsigned int LPSC_num) {
unsigned int j;
if( (*(unsigned int*)(PSC0_MDSTAT+4 * LPSC_num) & 0x11F) != 0x103 ) {
*(unsigned int*) (PSC0_MDCTL+4*LPSC_num) = (*(unsigned int*) (PSC0_MDCTL+4*LPSC_num) & 0xFFFFFEE0) | 0x0103;
PSC0_PTCMD = 0x1<<PD;
j = 0;
/*Wait for power state transition to finish*/
while( (PSC0_PTSTAT & (0x1<<PD) ) !=0) {
if( j++ > PSC_TIMEOUT ) {
GEL_TextOut("\tPSC0 Enable Core Transition Timeout on Domain %d, LPSC %d\n","Output",1,1,1,PD,LPSC_num);
break;
}
}
j = 0;
while( (*(unsigned int*)(PSC0_MDSTAT+4 * LPSC_num) & 0x11F) !=0x103) {
if( j++ > PSC_TIMEOUT ) {
GEL_TextOut("\tPSC0 Enable Core Verify Timeout on Domain %d, LPSC %d\n","Output",1,1,1,PD,LPSC_num);
break;
}
}
}
}
/*SyncReset Function for PSC0*/
PSC0_LPSC_SyncReset(unsigned int PD, unsigned int LPSC_num) {
unsigned int j;
if( (*(unsigned int*)(PSC0_MDSTAT+4 * LPSC_num) & 0x1F) != 0x1 ) {
*(unsigned int*) (PSC0_MDCTL+4*LPSC_num) = (*(unsigned int*) (PSC0_MDCTL+4*LPSC_num) & 0xFFFFFFE0) | 0x0001;
PSC0_PTCMD = 0x1<<PD;
j = 0;
/*Wait for power state transition to finish*/
while( (PSC0_PTSTAT & (0x1<<PD) ) !=0) {
if( j++ > PSC_TIMEOUT ) {
GEL_TextOut("\tPSC0 Sync Reset Transition Timeout on Domain %d, LPSC %d\n","Output",1,1,1,PD,LPSC_num);
break;
}
}
j = 0;
while( (*(unsigned int*)(PSC0_MDSTAT+4 * LPSC_num) & 0x1F) !=0x1) {
if( j++ > PSC_TIMEOUT ) {
GEL_TextOut("\tPSC0 Sync Reset Verify Timeout on Domain %d, LPSC %d\n","Output",1,1,1,PD,LPSC_num);
break;
}
}
}
}
/*Enable Function for PSC0*/
PSC0_LPSC_enable(unsigned int PD, unsigned int LPSC_num) {
unsigned int j;
if( (*(unsigned int*)(PSC0_MDSTAT+4 * LPSC_num) & 0x1F) != 0x3 ) {
*(unsigned int*) (PSC0_MDCTL+4*LPSC_num) = (*(unsigned int*) (PSC0_MDCTL+4*LPSC_num) & 0xFFFFFFE0) | 0x0003;
PSC0_PTCMD = 0x1<<PD;
j = 0;
/*Wait for power state transition to finish*/
while( (PSC0_PTSTAT & (0x1<<PD) ) !=0) {
if( j++ > PSC_TIMEOUT ) {
GEL_TextOut("\tPSC0 Enable Transition Timeout on Domain %d, LPSC %d\n","Output",1,1,1,PD,LPSC_num);
break;
}
}
j = 0;
while( (*(unsigned int*)(PSC0_MDSTAT+4 * LPSC_num) & 0x1F) !=0x3) {
if( j++ > PSC_TIMEOUT ) {
GEL_TextOut("\tPSC0 Enable Verify Timeout on Domain %d, LPSC %d\n","Output",1,1,1,PD,LPSC_num);
break;
}
}
}
}
/**********************************************************************************
DDR Configuration routine:
1. DDR Enable
2. VTP calibration
3. Configure DDR
4. Set to self-refresh, enable mclkstop and DDR Sync Reset
5. Enable DDR and disable self-refresh
int freq is MHz
DDR2 = 0
MDDR = 1
A DDR configuration spreadsheet tool is located here:
http://processors.wiki.ti.com/index.php/Programming_mDDR/DDR2_EMIF_on_OMAP-L1x/C674x
***********************************************************************************/
DEVICE_DDRConfig(unsigned int ddr_type, unsigned int freq)
{
unsigned int j;
unsigned int tmp_SDCR;
// Enable the Clock to EMIFDDR SDRAM
PSC1_LPSC_enable(PD0, LPSC_DDR);
// Begin VTP Calibration
VTPIO_CTL &= ~0x00000040; // Clear POWERDN
VTPIO_CTL &= ~0x00000080; // Clear LOCK
VTPIO_CTL |= 0x00002000; // Set CLKRZ in case it was cleared before (VTP looks for CLKRZ edge transition)
VTPIO_CTL &= ~0x00002000; // Clear CLKRZ (Use read-modify-write to ensure 1 VTP cycle wait for previous instruction)
VTPIO_CTL |= 0x00002000; // Set CLKRZ (Use read-modify-write to ensure 1 VTP cycle wait for previous instruction)
j = 0;
// Polling READY bit to see when VTP calibration is done
while((VTPIO_CTL & 0x00008000) == 0) {
if( j++ > VTP_TIMEOUT ) {
GEL_TextOut("\tVTP Ready timeout\n","Output",1,1,1);
break;
}
}
VTPIO_CTL |= 0x00000080; // Set LOCK bit for static calibration mode
VTPIO_CTL |= 0x00000040; // Set POWERDN bit to power down VTP module
// End VTP Calibration
VTPIO_CTL |= 0x00004000; // Set IOPWRDN to allow powerdown of input receivers when PWRDNEN is set
// **********************************************************************************************
// Setting based on the looser of 512Mb mDDR MT46H32M16LFBF-6,
// 1Gb mDDR MT46H64M16LF-6, or
// 1Gb mDDR MT46H64M16LFBF-6 on EVM
// Config DDR timings
DRPYC1R = (0x0 << 8) | // Reserved
(0x1 << 7) | // EXT_STRBEN
(0x1 << 6) | // PWRDNEN
(0x0 << 3) | // Reserved
(0x4 << 0); // RL
// DRPYC1R Value = 0x000000C4
if( DDR_DEBUG ) {
// Configure EMIF with max timings for more slack
// Try this if memory is not stable
DRPYC1R |= 0x7; // RL
}
// Settings that change depending on DDR2 or MDDR
if( ddr_type == DDR2 ) {
DDR_SLEW = 0x00000000; // Disable Pull Downs, Disable LVCMOS Rx
tmp_SDCR = (0x0 << 25) | // MSDRAMEN
(0x1 << 20); // DDR2EN
GEL_TextOut("\tUsing DDR2 settings\n","Output",1,1,1);
}
else if( ddr_type == MDDR ) {
DDR_SLEW = 0x00000030; // Enable Pull Downs, Enable LVCMOS Rx
tmp_SDCR = (0x1 << 25) | // MSDRAMEN
(0x0 << 20); // DDR2EN
GEL_TextOut("\tUsing mDDR settings\n","Output",1,1,1);
}
else {
DDR_SLEW = 0x00000030; // Enable Pull Downs, Enable LVCMOS Rx
tmp_SDCR = (0x1 << 25) | // MSDRAMEN
(0x0 << 20); // DDR2EN
GEL_TextOut("\tUnknown DDR Type! Using MDDR settings\n","Output",1,1,1);
}
EMIFDDR_SDCR |= 0x00800000; // Set BOOTUNLOCK
EMIFDDR_SDCR = tmp_SDCR | // Settings that change depending on DDR2 or MDDR
(EMIFDDR_SDCR & 0xF0000000) | // Reserved
(0x0 << 27) | // DDR2TERM1
(0x0 << 26) | // IBANK_POS
(0x0 << 24) | // DDRDRIVE1
(0x0 << 23) | // BOOTUNLOCK
(0x0 << 22) | // DDR2DDQS
(0x0 << 21) | // DDR2TERM0
(0x0 << 19) | // DDRDLL_DIS
(0x0 << 18) | // DDRDRIVE0
(0x1 << 17) | // DDREN
(0x1 << 16) | // SDRAMEN
(0x1 << 15) | // TIMUNLOCK
(0x1 << 14) | // NM
(0x0 << 12) | // Reserved
(0x3 << 9) | // CL
(0x0 << 7) | // Reserved
(0x2 << 4) | // IBANK
(0x0 << 3) | // Reserved
(0x2 << 0); // PAGESIZE
// mDDR SDCR Value = 0x02034622
if( ddr_type == MDDR ) {
EMIFDDR_SDCR2 = 0x00000000; // IBANK_POS set to 0 so this register does not apply
}
if( DDR_DEBUG ) {
// Configure EMIF with max timings for more slack
// Try this if memory is not stable
EMIFDDR_SDTIMR1 = (0x7F << 25) | // tRFC
(0x07 << 22) | // tRP
(0x07 << 19) | // tRCD
(0x07 << 16) | // tWR
(0x1F << 11) | // tRAS
(0x1F << 6) | // tRC
(0x07 << 3) | // tRRD
(EMIFDDR_SDTIMR1 & 0x4) | // Reserved
(0x03 << 0); // tWTR
EMIFDDR_SDTIMR2 = (EMIFDDR_SDTIMR2 & 0x80000000) | // Reserved
(((unsigned int) ((70000 / 7812.5) - 0.5)) << 27) | // tRASMAX
(0x3 << 25) | // tXP
(0x0 << 23) | // tODT (Not supported)
(0x7F << 16) | // tXSNR
(0xFF << 8) | // tXSRD
(0x07 << 5) | // tRTP (1 Cycle)
(0x1F << 0); // tCKE
// SDTIMR1 Value = 0xFFFFFFFB
// SDTIMR2 Value = 0x467FFFFF
GEL_TextOut("\tDDR Timings Configured for Debug\n","Output",1,1,1);
}
else {
// Let float -> integer truncate handle minus 1; Safer to round up for timings
EMIFDDR_SDTIMR1 = (((unsigned int) (110.0 * freq / 1000)) << 25) | // tRFC
(((unsigned int) ( 18.0 * freq / 1000)) << 22) | // tRP
(((unsigned int) ( 18.0 * freq / 1000)) << 19) | // tRCD
(((unsigned int) ( 15.0 * freq / 1000)) << 16) | // tWR
(((unsigned int) ( 42.0 * freq / 1000)) << 11) | // tRAS
(((unsigned int) ( 60.0 * freq / 1000)) << 6) | // tRC
(((unsigned int) ( 12.0 * freq / 1000)) << 3) | // tRRD
(EMIFDDR_SDTIMR1 & 0x4) | // Reserved
((2 - 1) << 0); // tWTR
EMIFDDR_SDTIMR2 = (EMIFDDR_SDTIMR2 & 0x80000000) | // Reserved
(((unsigned int) ((70000 / 7812.5) - 1)) << 27) | // tRASMAX
(0x3 << 25) | // tXP (Should be 6-1 per MT46H64M16LFBF-6 datasheet, but field only goes up to 0b11)
(0x0 << 23) | // tODT (Not supported)
(((unsigned int) (138.0 * freq / 1000)) << 16) | // tXSNR (tXSR for mDDR)
(((unsigned int) (138.0 * freq / 1000)) << 8) | // tXSRD (tXSR for mDDR)
((2 - 1) << 5) | // tRTP
((1 - 1) << 0); // tCKE
// SDTIMR1 Value @ 150MHz = 0x20923249
// SDTIMR2 Value @ 150MHz = 0x3E141420
}
EMIFDDR_SDCR &= ~0x00008000; // Clear TIMUNLOCK
// Let float -> integer truncate handle RR round-down; Safer to round down for refresh rate
EMIFDDR_SDRCR = (0x1 << 31) | // LPMODEN (Required for LPSC SyncReset/Enable)
(0x1 << 30) | // MCLKSTOPEN (Required for LPSC SyncReset/Enable)
(0x0 << 24) | // Reserved
(0x0 << 23) | // SR_PD
(0x0 << 16) | // Reserved
(((unsigned int) (7.8125 * freq)) << 0); // RR
// SyncReset the Clock to EMIFDDR SDRAM
PSC1_LPSC_SyncReset(PD0, LPSC_DDR);
// Enable the Clock to EMIFDDR SDRAM
PSC1_LPSC_enable(PD0, LPSC_DDR);
// Disable self-refresh
EMIFDDR_SDRCR &= ~0xC0000000;
// SDRCR Value @ 150MHz = 0x00000493
// Set PBBPR to a value lower than default to prevent blocking
EMIFDDR_PBBPR = 0x30;
}
/* DSP/BIOS Configuration Script for System 8000 Scanner */
/* Platform */
/*
utils.loadPlatform("ti.platforms.evm6748");
*/
/*
utils.loadPlatform("ti.platforms.evmOMAPL138");
*/
utils.loadPlatform("myplatforms.System8000");
/* Imports*/
utils.importFile('ndk.tci');
utils.importFile('mcbsp.tci');
/* The following DSP/BIOS Features are enabled. */
bios.enableMemoryHeaps(prog);
bios.enableRealTimeAnalysis(prog);
bios.enableRtdx(prog);
bios.enableTskManager(prog);
/* create the NDK stack thread */
bios.tskNdkStackTest = bios.TSK.create("tskNdkStack");
bios.tskNdkStackTest.fxn = prog.extern("NetworkStack");
bios.tskNdkStackTest.stackSize = 0x1000;
bios.tskNdkStackTest.priority = 0x5;
/* Enable power management (required for psp drivers) */
/* See C6748_BIOSPSP_Userguide 1.6.1 */
bios.PWRM.ENABLE = 1;
bios.PWRM.RESOURCETRACKING = 1;
bios.PWRM.SCALING = 1;
/* Check that stack size is big enough for the application */
if (bios.MEM.STACKSIZE < 0x1000) {
bios.MEM.STACKSIZE += 0x1000;
}
/* Board specific settings */
bios.MEM.instance("IRAM").len = 0x0002ffff;
/* Create a heap in DDR external memory */
/*
bios.MEM.instance("DDR").createHeap = 1;
bios.MEM.instance("DDR").heapSize = 0x00010000;
bios.MEM.BIOSOBJSEG = prog.get("DDR");
bios.MEM.MALLOCSEG = prog.get("DDR");
*/
/* Create a heap in SDRAM external memory */
bios.MEM.instance("SDRAM").createHeap = 1;
bios.MEM.instance("SDRAM").heapSize = 0x00010000;
bios.MEM.BIOSOBJSEG = prog.get("SDRAM");
bios.MEM.MALLOCSEG = prog.get("SDRAM");
bios.GBL.C64PLUSL2CFG = "256k";
/* Configure Board */
bios.GBL.CLKOUT = 300.0000;
bios.GBL.CALLUSERINITFXN = 1;
bios.GBL.USERINITFXN = prog.extern("SYS_init");
/* Configure Logging servic for instrumentation */
bios.LOG.TS = true;
bios.LOG.create("DVTEvent_Log");
/*
bios.LOG.instance("DVTEvent_Log").bufSeg = prog.get("DDR");
*/
bios.LOG.instance("DVTEvent_Log").bufSeg = prog.get("SDRAM");
bios.LOG.instance("DVTEvent_Log").bufLen = 8192;
bios.LOG.instance("DVTEvent_Log").comment = "DVT";
bios.LOG.create("trace");
bios.LOG.instance("trace").bufLen = 1024;
bios.LOG.instance("trace").bufSeg = prog.get("IRAM");
/* Configure timer */
bios.CLK.TIMERSELECT = "Timer 0";
bios.CLK.RESETTIMER = true;
/* Move all sections to DDR external memory */
/*
bios.setMemCodeSections(prog, prog.get("DDR"));
bios.setMemDataHeapSections(prog, prog.get("DDR"));
bios.setMemDataNoHeapSections(prog, prog.get("DDR"));
*/
/* Move all sections to SDRAM external memory */
bios.setMemCodeSections(prog, prog.get("SDRAM"));
bios.setMemDataHeapSections(prog, prog.get("SDRAM"));
bios.setMemDataNoHeapSections(prog, prog.get("SDRAM"));
/* Remove IRAM since we've set L2 to be cache */
bios.IRAM.destroy();
/* Enable ECM too for NDK interrupt manager to use if required */
bios.ECM.ENABLE = 1;
/* ECM Configuration */
bios.HWI.instance("HWI_INT7").interruptSelectNumber = 0;
bios.HWI.instance("HWI_INT8").interruptSelectNumber = 1;
bios.HWI.instance("HWI_INT9").interruptSelectNumber = 2;
bios.HWI.instance("HWI_INT10").interruptSelectNumber = 3;
/*task configuration*/
bios.TSK.create("taskMcBspInput");
bios.TSK.instance("taskMcBspInput").stackSize = 4096;
bios.TSK.instance("taskMcBspInput").priority = 14;
bios.TSK.instance("taskMcBspInput").fxn = prog.extern("mcbspInputTask");
bios.TSK.instance("taskMcBspInput").comment = "McBsp Input Task";
bios.TSK.create("taskMcBspOutput");
bios.TSK.instance("taskMcBspOutput").stackSize = 4096;
bios.TSK.instance("taskMcBspOutput").priority = 14;
bios.TSK.instance("taskMcBspOutput").fxn = prog.extern("mcbspOutputTask");
bios.TSK.instance("taskMcBspOutput").comment = "McBsp Output Task";
/* Create Semaphores */
bios.SEM.create("SEM_EVENT_DATA");
bios.SEM.instance("SEM_EVENT_DATA").comment = "Event Semaphore: output data is ready to send to host";
bios.SEM.create("SEM_EVENT_NETWORKREADY");
bios.SEM.instance("SEM_EVENT_NETWORKREADY").comment = "Indicates the network is done initializing";
bios.TSK.create("taskTest");
bios.TSK.instance("taskTest").order = 1;
bios.TSK.instance("taskTest").priority = 8;
/*
bios.TSK.instance("taskTest").fxn = prog.extern("task_Test", "asm");
*/
bios.TSK.instance("taskTest").fxn = prog.extern("task_Test");
bios.TSK.instance("taskTest").comment = "Test task";
// !GRAPHICAL_CONFIG_TOOL_SCRIPT_INSERT_POINT!
if (config.hasReportedError == false) {
prog.gen();
}
/*
* Copyright (c) 2011 by Texas Instruments and others.
* All rights reserved. This program and the accompanying materials
* are made available under the terms of the Eclipse Public License v1.0
* which accompanies this distribution, and is available at
* http://www.eclipse.org/legal/epl-v10.html
*
* Contributors:
* Texas Instruments - initial implementation
*
* */
/*
* ======== Platform.tci ========
*
*/
/*
* The following comment is used by the Graphical Config Tool:
* !DESCRIPTION 6XXX! System8000 (300 MHz) with 32 Mbytes SDRAM
* !NAME! System8000
*/
/*
* Setup platform-specific memory map, CLK rate, etc.
*/
var mem_ext = [];
mem_ext[0] = {
comment: "32 Mbytes of the DSP's off-chip memory",
name: "SDRAM",
base: 0x40000000,
len: 0x02000000,
space: "code/data"
};
/* Specify the L1 and L2 memory settings */
var device_regs = {
l1PMode: "32k",
l1DMode: "32k",
l2Mode: "0k"
};
var params = {
clockRate: 300,
catalogName: "ti.catalog.c6000",
deviceName: "6748",
regs: device_regs,
mem: mem_ext
};
/* override the defaults with anything specified by client */
if (utils.loadPlatform.params != null) {
var overrides = utils.loadPlatform.params;
for (var i in params) {
if (i in overrides) {
params[i] = overrides[i];
}
}
}
/*
* Customize generic platform with parameters specified above.
*/
utils.loadPlatform("ti.platforms.generic", params);
/*
* @(#) ti.platforms.evm6748; 1, 0, 0,130; 1-17-2011 09:12:37; /db/ztree/library/trees/platform/platform-l32x/src/
*/
Mary