This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM4376: ti-processor-sdk-linux-am437x-hs-evm-06.03.00.106

Part Number: AM4376

CVEs details- In Das U-Boot through 2022.07-rc5, an integer signedness error and resultant stack-based buffer overflow in the "i2c md" command enables the corruption of the return address pointer of the do_i2c_md function. nvd.nist.gov/.../CVE-2022-34835 Patched details- lists.denx.de/.../486113.html Can you reconfirm if this CVEs is been fixed/mitigated from TI-U boot code shared.