I am setting up Intel realsense camera on TDA4VM following this https://software-dl.ti.com/jacinto7/esd/robotics-sdk/08_06_01/TDA4VM/docs/source/docs/realsense_driver_node.html# link and have set up the Librealsense library and realsense-ros library but facing this issue while running roslaunch realsense2_camera rs_camera.launch
NODES
/camera/
realsense2_camera (nodelet/nodelet)
realsense2_camera_manager (nodelet/nodelet)
auto-starting new master
process[master]: started with pid [869]
ROS_MASTER_URI=http://localhost:11311
setting /run_id to 2d6b24c4-5679-11ee-a10f-0242ac110002
process[rosout-1]: started with pid [880]
started core service [/rosout]
process[camera/realsense2_camera_manager-2]: started with pid [887]
process[camera/realsense2_camera-3]: started with pid [888]
[ INFO] [1695078896.497300252]: Initializing nodelet with 2 worker threads.
[ INFO] [1695078896.800310892]: RealSense ROS v2.3.2
[ INFO] [1695078896.800837120]: Built with LibRealSense v2.50.0
[ INFO] [1695078896.801437017]: Running with LibRealSense v2.50.0
[ INFO] [1695078896.846436854]:
[ WARN] [1695078896.873789862]: Device 1/1 failed with exception: failed to set power state
[ERROR] [1695078896.874195870]: The requested device with is NOT found. Will Try again.
18/09 23:14:56,872 ERROR [281472847896944] (handle-libusb.h:51) failed to open usb interface: 0, error: RS2_USB_STATUS_NO_DEVICE
18/09 23:14:56,872 ERROR [281472873075056] (sensor.cpp:572) acquire_power failed: failed to set power state
18/09 23:14:56,873 WARNING [281472873075056] (rs.cpp:310) null pointer passed for argument "device"