Other Parts Discussed in Thread: AM1808, AM1707
Hello,
I need your help obtaining the schematics for the AM1707EVM board. I am using the LAN8710A 10/100 PHY, and need help with the connections. However, I can’t download the board schematics from the Logic PD website because I haven't purchased a board. I just need to know how the EVM is connected, so that I can use it in my design. I got the schematics from the AM1808 board, but it’s unclear if the outputs match up with the AM1707. If you confirm that they do, then I am set; otherwise, I need the schematics for the AM1707.
http://focus.ti.com/docs/toolsw/folders/print/tmdxevm1707.html
TMDXEVM1707
-David