Part Number: SK-AM64B
Hello,
Question of how to configure TCA6424ARGJR for POWER ON (POR) BOOTMODE without using external TEST AUTOMATION connector in the real design ?
Requirement of changing BOOTMODE from UART to OSPI and vice versa etc. by configuring the I2C IO Expander device above. The programming of the device for the proper IO level
is done before the POR cycle is initiated (under SoC/MCU I2C control). But if the power is recycled then the IO of the device is Hi-Z and Input direction as per spec and the previously programmed
information is lost.
So how the proper IO signal levels are retained in the POR ? Or will it work only in WARM Reset mode only and P/S has to be maintained ?
Will Warm Reset work in BOOTMODE as well as in Hard Reset ?
Thanks