This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Flash Booting issues on C6713

Hi,

I am using a board with DSP C6713 and a parallel flash. I want to boot from Flash and have a couple of questions.

The Bootmode pins are HD4 and HD3 and for the device to boot from Flash, HD4=0, HD3=1.

The datasheet says that HD4 has a IPD and HD3 has a IPU. Is this sufficient?

Or do we add external PUs and PDs?

Also in the following post

http://e2e.ti.com/support/dsp/tms320c6000_high_performance_dsps/f/115/t/86746.aspx

they talk about adding a pull-up on GP[13] for proper operation.

Is this still required?

Thanks,

Aditi.