Other Parts Discussed in Thread: TDA4VH
hi,experts
I am currently using the TDA4VH development board with SDK 8.6. I used the switch mode in native driver for testing.
When I was testing the features of CBS,I saw the following article
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1233877/dra821-cpsw-cbs-configuration-and-linux-standard-tc-cbs-interface?tisearch=e2e-sitesearch&keymatch=CBS#

The article mentions that both standard CBS shaping and the method of using “shaper bw_rlimit” with “min rate” and “max rate” are supported.
I would like to verify the standard CBS configuration, so I used the following command to configure the CBS queue.
ifconfig eth1 down
ifconfig eth2 down
ifconfig eth3 down
ifconfig eth4 down
ethtool -L eth2 tx 8
ethtool --set-priv-flags eth2 p0-rx-ptype-rrobin off
devlink dev param set platform/c000000.ethernet name switch_mode value true cmode runtime
ip link add name br0 type bridge
ip link set dev br0 type bridge ageing_time 1000
ip link set dev eth1 up
ip link set dev eth2 up
ip link set dev eth3 up
ip link set dev eth4 up
ip link set dev eth1 master br0
ip link set dev eth2 master br0
ip link set dev eth3 master br0
ip link set dev eth4 master br0
ifconfig br0 up
bridge vlan add dev eth1 vid 11 master
bridge vlan add dev eth2 vid 11 master
bridge vlan add dev eth3 vid 11 master
bridge vlan add dev eth4 vid 11 master
tc qdisc add dev eth2 handle 100: parent root mqprio num_tc 8 \
map 0 1 2 3 4 5 6 7 0 0 0 0 0 0 0 0 \
queues 1@0 1@1 1@2 1@3 1@4 1@5 1@6 1@7 \
hw 0
tc qdisc replace dev eth2 parent 100:1 cbs \
locredit -1470 hicredit 30 sendslope -980000 idleslope 20000
tc qdisc replace dev eth2 parent 100:2 cbs \
locredit -1470 hicredit 30 sendslope -980000 idleslope 20000
tc qdisc replace dev eth2 parent 100:3 cbs \
locredit -1470 hicredit 30 sendslope -980000 idleslope 20000
tc qdisc replace dev eth2 parent 100:4 cbs \
locredit -1470 hicredit 30 sendslope -980000 idleslope 20000
tc qdisc replace dev eth2 parent 100:5 cbs \
locredit -1470 hicredit 30 sendslope -980000 idleslope 20000
tc qdisc replace dev eth2 parent 100:6 cbs \
locredit -1470 hicredit 30 sendslope -980000 idleslope 20000
tc qdisc replace dev eth2 parent 100:7 cbs \
locredit -1470 hicredit 30 sendslope -980000 idleslope 20000
tc qdisc replace dev eth2 parent 100:8 cbs \
locredit -1470 hicredit 30 sendslope -980000 idleslope 20000
When I test the bandwidth using iperf, it does not achieve the desired bandwidth limitation effect.

So please tell me, how can I correctly use CBS configuration?