Other Parts Discussed in Thread: TDA4VL, TDA4VM
We plan to use trace32 to flash and debug our TDA4AL board, but currently we have encountered some issues:
1.The trace32 we are currently using is an ARM-26->TI-16 Pin connector, and our TDA4AL board has reserved a 10Pin interface. Our wiring diagram has been uploaded to the attachment (TI-16_TDA4AL-10 Pin_connect), and we need help to confirm if it is correct.
2. Currently, when we use TRACE32 software to debug the TDA4 board, there will be a debug port failed error, and then click CPU ->System Settings ->DETECT to run. However, once executed the file _J721S2_allcoretypes_connect.cmm will report error "debug port failed", Could you please confirm if this issue is related to the license or other issues? Please refer to the attached issue_video.mp4.