Part Number: J721S2XSOMXEVM
Hi,
SDK Version: 8.6
core : mcu2_1
The MCAL example code PwmApp_Gpt fails to generate an interrupt in one-shot mode and has no waveform output in one-shot mode
After modifying PwmApp_Gpt according to the patch provided by TI, waveforms can be output and interrupts can be generated normally in AUTOLOAD mode.
0001-TIMEROI1-output-PWM-on-AG25-ball-to-TP82.zip
But when I changed TIMER_AUTORLD_NOCMP_ENABLE in mcusw/mcal_drv/mcal/Pwm/src/Pwm_Gptimer.c to TIMER_ONESHOT_NOCMP_ENABLE, When TIMER_AUTORLD_CMP_ENABLE was changed to TIMER_ONESHOT_CMP_ENABLE, it was found that GPTimer failed to generate interrupts
Here is the log for one-shot mode

Please ask the experts of TI to help modify the code to verify this problem
Regards,
bingxian