Hi TI experts
I am researching how to obtain H3A data.Encountering some unclear points, I would like to ask for advice.


The first image is H3A data and the second image is my own statistics based on my understanding of H3A data statistics in the raw image.
The statistical process is as follows:
1.Obtain a 12bit RAW image from DCC
2.Restore a 12bit image to 24bit through PWL decompression

3.The above parameters are set to 5 and extract 10 bits from the 9th bit of a 24bit image.
4.Set the same block area as H3A based on the .bin file
5.Calculate the cumulative sum of block regions
6.Using 16bit data to save cumulative sum
Why these two pictures are different?