This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

flash boot utility sfh_OMAP-L137

Other Parts Discussed in Thread: OMAP-L137, OMAPL138, OMAP-L138

Hi, I tried sfh_OMAP-L137.exe and have some question. I have written to moridinga at users.sourceforge.net but I received no response.

is it possible without modification of SFH to flash SPI EEPROM via SPI1? I have not found the option for this.

is there some size limit for binary application file for sfh_omap-L137 - flash_noubl option? My BIN file has several MBytes.

is there any way how to use UART boot with 25MHz input clock (my ROM version is  d800k003)? 

Thanks