Hello, everybody!
Now we are debugging the TMDXEVM6670L, as you know, the 4 Serial RapidIO lanes, 2 PCIe lanes, 1 SGMII port and 6 AIF2 lanes of C6670 are all routed to AMC edge connector.To debug and evaluate these peripherals, we decide to design an AMC compatible carrier board, namely a conversion card , which shall be used for connecting one EVM to another or each EVM can be tested in loopback mode, so that we can do more tests, such as the chip to chip SRIO communication....
Here we are confused with one key question, the AIF2 input pins RP1 CLK, RP1 FB, PHYSYNC and RADSYNC also are routed to AMC edge connector, but how should we trigger them? In my opinion, if we do nothing for these pins, the AIF2 timer won't work. so some essential design should be considered.
Does anyone have realize such a design? can you give me some advices?
Any proposal will be greatly appreciated! Thank you!
Tao