This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDXEVM3358: Flashing SPI with Uniflash

Part Number: TMDXEVM3358
Other Parts Discussed in Thread: UNIFLASH

Hi

I am struggling in flashing the SPI Flash of TMDXEVM3358 over UART interface.
I flashed the MLO file generated with [Processor SDK SITARA AM335X Linux Package v08.02.00.24] using Uniflash v8.4.0 on win10(64bit).
Then after flushing 2% of the MLO file it failed.

The steps carried out are:

1. dslite.bat --mode processors -c COM10 -f C:\ti\uniflash_8.4.0\processors\FlashWriter\evmAM335x\uart_evmAM335x_flash_programmer.bin -i 0
    Executing the following command:
    > C:\ti\uniflash_8.4.0\processors\ProcessorSDKSerialFlash.exe -c COM10 -f C:\ti\uniflash_8.4.0\processors\FlashWriter\evmAM335x\uart_evmAM335x_flash_programmer.bin -i 0

    For more details and examples, please refer to the UniFlash Quick Start guide.


    ----------------------------------------------------------------------------
    ProcessorSDKSerialFlash CLI Tool
    Copyright (C) 2017-2023 Texas Instruments Incorporated - http://www.ti.com/
    Version 1.10.0.0
    ----------------------------------------------------------------------------
    Downloading Flash Programmer..

    Transferring File of size 47896 bytes
    File Transfer complete!


2. dslite.bat --mode processors -c COM10 -f C:\ti\sample\MLO.bin-d 1 -i 1 -o 0
    Executing the following command:
    > C:\ti\uniflash_8.4.0\processors\ProcessorSDKSerialFlash.exe -c COM10 -f C:\ti\sample\MLO.bin-d 1 -i 1 -o 0

    For more details and examples, please refer to the UniFlash Quick Start guide.


    ----------------------------------------------------------------------------
    ProcessorSDKSerialFlash CLI Tool
    Copyright (C) 2017-2023 Texas Instruments Incorporated - http://www.ti.com/
    Version 1.10.0.0
    ----------------------------------------------------------------------------
    Transferring the Image to Flash Programmer..

    Transferring Header Information..
    Header Transfer Complete!

    Flashing Image of size 109612 bytes
    2% complete
    Flash Programming Failed!!

Could you please tell me what is wrong?