Hi,
My customer would like to ask you a question about the rise timing of the AM6442 reset signal.
Specifically, it is about the interval at which MCU_RESETSTATz and RESETSTATz rise after MCU_RESETz rises.
The following timings are specified in the page 119 of the data sheet.
- RST12 (Delay time, MCU_RESETz inactive (high) to MCU_RESETSTATz inactive (high)) : Min 38.64us (calculated at a clock frequency of 25MHz)
- RST14 (Delay time, MCU_RESETz inactive (high) to RESETSTATz inactive (high)) : Min 161.6us (calculated at a clock frequency of 25MHz)
However, these actual measured values were 24.38us for RST12 and 145.6us for RST14 which are smaller than the minimum values described in the above table when they actually measured these timings.
Could you please confirm the reason for these differences?
They are concerned about individual differences between devices and the possibility of typo in the data sheets (for example, min and max may be exchanged).
Thanks and regards,
Hideaki