This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5718: USB 2.0 Host transmit specification

Genius 3186 points

Part Number: AM5718

Hi

May I have a question about AM5718 USB 2.0 host mode Voltage specification?

My customer is testing eye-pattern of USB.

In AM5718 is Host, transmit. the  voltage level was +-575mV.

I think this is not probrem for device, However transmitter specification is +-525mV.

Is there any USB 2.0 test report for AM5718?

And Is there any setting transmit voltage level config +-525mV or +-475mV?

Thanks,

GR