Hi,
I want to create a secondary bootloader for C6713 DSP.
I am using the SPRA999A document form TI for this purpose.
The document suggests to create and link the copy table as follows
.text : load = FLASH_REST, run = IRAM, table(BINIT)
.const : load = FLASH_REST, run = IRAM, table(BINIT)
I have used the same in my linker command file. BUt when I compile the project, the compiler
throws a warning :
warning: table(BINIT) operator ignored for ".text":
   table() operator cannot be associated with empty output section
 warning: table(BINIT) operator ignored for ".const": 
   table() operator cannot be associated with empty output section
I cannot see any .binit section in the MAP file.
What do these warnings mean? And how can I resolve the issue?
Thanks,
Aditi.