This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VH-Q1: Current injection on Analog inputs

Part Number: TDA4VH-Q1

Hello E2E,

In the TDA4VH-Q1 datasheet, SPRSP79 – FEBRUARY 2023

It is specified in the absolute maximum ratings (sec 7.1) that "For current pulse injection:
Pins stressed per JEDEC JESD78E (Class II) and passed with specified I/O pin injection current and clamp voltage of 1.5 times
maximum recommended I/O voltage and negative 0.5 times maximum recommended I/O voltage.
For overvoltage performance:
Supplies stressed per JEDEC JESD78E (Class II) and passed specified voltage injection."

Does this also include Analog input pins(ADC channels) on the TDA? In sec 7.1 it just says latch up performance with note(5). Unsure if this also applies for analog input pins?

Sincerely,
Leelakrishna Koneti