Part Number: AM5706
Hello,
My cusotmer has a question for CS configuration in GPMC.
Now they are using 3 CS area like the below.
CS0 0x0800_0000 ~ 0x09FF_FFFF
CS2 0x1800_0000 ~ 0x1FFF_FFFF
CS3 0x1000_0000 ~ 0x17FF_FFFF
CS3 is assinged to smaller address than CS2.
Is this configuration, larger number of CS area is assigned to smaller address area than smaller number of CS area, allowed?
In this configuration, when trying to access to CS3 area, they can’t see any GPMC signal outputs from the device.
So somthing must be wrong.
The below is their configuration for CS2 and CS3.
CONFIG1_0 0x0000_1000
CONFIG2_0 0x0008_1080
CONFIG3_0 not changed
CONFIG4_0 0x0701_EF96
CONFIG5_0 0x010F_0911
CONFIG6_0 0x0F07_0000
CONFIG7_0 0x0000_0E48 or 0x0000_0848
CONFIG1_2 0x0060_1000
CONFIG2_2 0x0007_0700
CONFIG3_2 not changed
CONFIG4_2 0x0601_E602
CONFIG5_2 0x0106_0B0A
CONFIG6_2 0x0707_0000
CONFIG7_2 0x0000_0858
CONFIG1_3 0x0000_1000
CONFIG2_3 0x0007_0B00
CONFIG3_3 not changed
CONFIG4_3 0x0601_EA01
CONFIG5_3 0x0109_070E
CONFIG6_3 0x0507_0000
CONFIG7_3 0x0000_0850
Do you see anything wrong?
Regards,
Oba