Hi all
I read reference manual from http://www.ti.com/lit/ug/sprugz8/sprugz8.pdf page 123
this page says the ocmc from 0x40400000h will use to download image when use Peripheral Boot
but in
http://www.ti.com/lit/ds/symlink/tms320dm8148.pdf
This address is resolved
And from http://www.ti.com/lit/ds/symlink/tms320c6a8168.pdf page 26 says this is the other 128k ocmc sram
Can I consider that the dm8148 also have the 256K SRAM ? the 40400000h address is useable for the ocmc sram just same as 8168 ?
thanks and best regards