This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62A-LP: SPI Flash Dependency?

Part Number: SK-AM62A-LP

Hello experts and enthusiasts,

I am getting close to building a custom board based off of the SK-AM62A-LP board and would like to confirm that the MCU or anything isn't reliant on the OSPI Flash (i.e. for booting or running). I see that a U-boot centric layout is created by Device Tree but the mtdblocks are of type NAND in Linux (and believe that they aren't formatted with UBI or the like) so I can't tell that there is any data on it. It seems to just be an alternative boot and storage device but since I wish to leave it out of my design I would like to confirm that there is no need for it.

Thank you,

Steve T