This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

timer



good day
I took the example of a timer that was in the folder cslr, follows the same if possible abaixo.Gostaria me explain the four states that have in one section of the program.

#define TIMER_EVENT0   04
#define TIMER_EVENT1   64       That is want to know what these numbers mean 04.64,40,48.
#define TIMER_EVENT2   40
#define TIMER_EVENT3   48

 

#include <stdio.h>
#include <c6x.h>
#include <ti/pspiom/cslr/csl_types.h>
#include <ti/pspiom/cslr/cslr_intc.h>
#include <ti/pspiom/cslr/soc_C6747.h>
#include <ti/pspiom/cslr/cslr_tmr.h>
#include <ti/pspiom/cslr/cslr_syscfg_C6747.h>



const unsigned int TIMER_PERIOD = 0x00001000;

static void device_init(void);
static void setup_TIMER0(void);
static void setup_TIMER1(void);
static void delay(Uint32 count);
static void test_TIMERS(void);

void myExit(int);
void test_TIMERS(void);

void TIMER0_TINT12_isr();
void TIMER0_TINT34_isr();
void TIMER1_TINT12_isr();
void TIMER1_TINT34_isr();

volatile int TIMER0_TINT12_status = 1;          // Pass/Fail flag
volatile int TIMER0_TINT34_status = 1;          // Pass/Fail flag
volatile int TIMER1_TINT12_status = 1;          // Pass/Fail flag
volatile int TIMER1_TINT34_status = 1;          // Pass/Fail flag
volatile int test_status = 1;                   // Test status

CSL_TmrRegsOvly tmr0Regs = (CSL_TmrRegsOvly)CSL_TMR_0_REGS;
CSL_TmrRegsOvly tmr1Regs = (CSL_TmrRegsOvly)CSL_TMR_1_REGS;

extern const unsigned int TIMER_PERIOD;

/* DSP interrupt events for the Timers  */
#define TIMER_EVENT0   04
#define TIMER_EVENT1   64
#define TIMER_EVENT2   40
#define TIMER_EVENT3   48


/*============================================================================*/
/*                        EXTERNAL FUNCTION PROTOTYPES                        */
/*============================================================================*/

extern void intcVectorTable(void);

/*============================================================================*/
/*                            FUNCTION DEFINTIONS                             */
/*============================================================================*/

void main (void)
{
    /* Enable TIMER0 and TIMER1 in mux and psc                                */
    device_init();

    /* Configure TIMER0, both halves to be used by application                */
    setup_TIMER0();

    /* Configure TIMER1 as dual 32 bit unchained timers for use by application*/
    setup_TIMER1();

    /* function to test the timer interrupts                                  */
    test_TIMERS();
}


void setup_TIMER0 (void)
{
    /* Clear TIM12 register                        */
    CSL_FINST(tmr0Regs->TIM12,TMR_TIM12_TIM12,RESETVAL);

    /* Clear TIM34 register                        */
    CSL_FINST(tmr0Regs->TIM34,TMR_TIM34_TIM34,RESETVAL);

    /* Select 32 bit unchained mode                */
    /* Take the timer out of reset and set the pre-scalar count for 3:4       */
    tmr0Regs->TGCR = CSL_FMKT(TMR_TGCR_TIMMODE,32BIT_UNCHAIN)
                     | CSL_FMKT(TMR_TGCR_TIM12RS,NO_RESET)
                     | CSL_FMKT(TMR_TGCR_TIM34RS,NO_RESET)
                     | CSL_FMK(TMR_TGCR_PSC34,0x1);

    /* Set timer0 PRD1:2                           */
    CSL_FINS(tmr0Regs->PRD12,TMR_PRD12_PRD12,TIMER_PERIOD);

    /* Set timer0 PRD3:4                           */
    CSL_FINS(tmr0Regs->PRD34,TMR_PRD34_PRD34,TIMER_PERIOD);
}


void setup_TIMER1 (void)
{
    /* Clear TIM12 register                        */
    CSL_FINST(tmr1Regs->TIM12,TMR_TIM12_TIM12,RESETVAL);

    /* Clear TIM34 register                        */
    CSL_FINST(tmr1Regs->TIM34,TMR_TIM34_TIM34,RESETVAL);

    /* Select 32 bit unchained mode                                           *
     * Take the timer out of reset and set the pre-scalar count for 3:4       */
    tmr1Regs->TGCR = CSL_FMKT(TMR_TGCR_TIMMODE,32BIT_UNCHAIN)
                     | CSL_FMKT(TMR_TGCR_TIM12RS,NO_RESET)
                     | CSL_FMKT(TMR_TGCR_TIM34RS,NO_RESET)
                     | CSL_FMK(TMR_TGCR_PSC34,0x1);

    /* Set timer1 PRD1:2                           */
    CSL_FINS(tmr1Regs->PRD12,TMR_PRD12_PRD12,TIMER_PERIOD);

    /* Set timer1 PRD3:4                           */
    CSL_FINS(tmr1Regs->PRD34,TMR_PRD34_PRD34,TIMER_PERIOD);
}

static void test_TIMERS(void)
{
    /* Interrupt Controller Register Overlay                                  */
    CSL_IntcRegsOvly intcRegs = (CSL_IntcRegsOvly)CSL_INTC_0_REGS;

    printf("Testing TIMER0 and TIMER1 in unchained 32 bit mode.\n");
    printf("Starting TIMER0 3:4 side and TIMER1 1:2 and 3:4 sides.\n");

    /* connect the event to the interrupt 4,5,6 and 7                         */
    CSL_FINS(intcRegs->INTMUX1, INTC_INTMUX1_INTSEL4,TIMER_EVENT0);
    CSL_FINS(intcRegs->INTMUX1, INTC_INTMUX1_INTSEL5,TIMER_EVENT1);
    CSL_FINS(intcRegs->INTMUX1, INTC_INTMUX1_INTSEL6,TIMER_EVENT2);
    CSL_FINS(intcRegs->INTMUX1, INTC_INTMUX1_INTSEL7,TIMER_EVENT3);

    /* set ISTP to point to the vector table address                          */
    ISTP = (unsigned int)intcVectorTable;

    /* clear all interrupts, bits 4 thru 15                                   */
    ICR = 0xFFF0;

    /* enable the bits for non maskable interrupt and                         */
    IER = 0xF2;

    /* enable interrupts, set GIE bit                                         */
    _enable_interrupts();

    delay(100);

    /* Enable TIMER0 1:2 side, one shot mode                                  */
    CSL_FINST(tmr0Regs->TCR,TMR_TCR_ENAMODE12,EN_ONCE);

    /* Enable TIMER0 3:4 side, one shot mode                                  */
    CSL_FINST(tmr0Regs->TCR,TMR_TCR_ENAMODE34,EN_ONCE);

    /* Enable TIMER1 1:2 side, one shot mode                                  */
    CSL_FINST(tmr1Regs->TCR,TMR_TCR_ENAMODE12,EN_ONCE);

    /* Enable TIMER1 3:4 side, one shot mode                                  */
    CSL_FINST(tmr1Regs->TCR,TMR_TCR_ENAMODE34,EN_ONCE);

    /* Sleep for 3 system clock PRD's to ensure other timers have ran.        *
     * Since 3:4 sides are running at a divide by 2 PRD, we need to           *
     * sleep at least 2 PRDs.                                                 */
    delay(1000);

    do
    {
        /* Check if interrupts occurred       */
        test_status = TIMER0_TINT12_status
                        | TIMER0_TINT34_status
                        | TIMER1_TINT12_status
                        | TIMER1_TINT34_status;

        delay(1000);
    }while (test_status != 0);

    /* Call exit function                     */
    myExit(test_status);
}


interrupt void TIMER0_TINT12_isr()
{
    /* Disable TIMER0 1:2 side                */
    CSL_FINST(tmr0Regs->TCR,TMR_TCR_ENAMODE12,DISABLE);

    /* Set flag to 0 indicating ISR occurred  */
    TIMER0_TINT12_status=0;
}

interrupt void TIMER0_TINT34_isr()
{
    /* Disable TIMER0 3:4 side                */
    CSL_FINST(tmr0Regs->TCR,TMR_TCR_ENAMODE34,DISABLE);

    /* Set flag to 0 indicating ISR occurred  */
    TIMER0_TINT34_status=0;
}


interrupt void TIMER1_TINT12_isr()
{
    /* Disable TIMER1 1:2 side                */
    CSL_FINST(tmr1Regs->TCR,TMR_TCR_ENAMODE12,DISABLE);

    /* Set flag to 0 indicating ISR occurred  */
    TIMER1_TINT12_status=0;
}

interrupt void TIMER1_TINT34_isr()
{
    /*( Disable TIMER1 3:4 side   */
    CSL_FINST(tmr1Regs->TCR,TMR_TCR_ENAMODE34,DISABLE);

    /* Set flag to 0 indicating ISR occurred  */
    TIMER1_TINT34_status=0;
}

void myExit(int test_result)
{
    /* Disable TIMER0 1:2 side  */
    CSL_FINST(tmr0Regs->TCR,TMR_TCR_ENAMODE12,DISABLE);

    /* Disable TIMER0 3:4 side  */
    CSL_FINST(tmr0Regs->TCR,TMR_TCR_ENAMODE34,DISABLE);

    /* Disable TIMER1 1:2 side  */
    CSL_FINST(tmr1Regs->TCR,TMR_TCR_ENAMODE12,DISABLE);

    /* Disable TIMER1 3:4 side  */
    CSL_FINST(tmr1Regs->TCR,TMR_TCR_ENAMODE34,DISABLE);

    /* Turn off all interrupts  */
    _disable_interrupts();

    /* Display test status      */
    if (test_result == 0)
    {
        printf("Timer0 and Timer1 interrupt test: PASSED.\n");
    }
    else
    {
        printf("Timer0 and Timer1 interrupt test: FAILED.\n");
    }
    exit(0);
}



void device_init(void)
{
    CSL_SyscfgRegsOvly sysRegs = (CSL_SyscfgRegsOvly)CSL_SYSCFG_0_REGS;

    /* Key to be written to enable the pin mux registers to be written        */
    sysRegs->KICK0R = 0x83e70b13;
    sysRegs->KICK1R = 0x95A4F1E0;

    /* mux between Timer 0/1 and GPIO[8:11], enable Timer0/1                  */
    sysRegs->PINMUX8 = CSL_FMKT(SYSCFG_PINMUX8_PINMUX8_19_16,TM64P0_OUT12);

    /* lock the pinmux registers                                              */
    sysRegs->KICK0R = 0x00000000;
    sysRegs->KICK1R = 0x00000000;
}


/*
 * \brief    Function to introduce a delay in to the program.
 *
 * \param    count [IN]  delay count to wait
 * \return   None
 *
 */
static void delay(Uint32 count)
{
    volatile Uint32 tempCount = 0;

    for (tempCount = 0; tempCount < count; tempCount++)
    {
        /* dummy loop to wait for some time  */
    }
}

  • If you notice TIMER_EVENT0, TIMER_EVENT1, TIMER_EVENT2 and TIMER_EVENT3 are used by the CSL_FINS function. The declaration of the CSL_FINS function is as follows…. CSL_FINS(reg, field, val). In essence they are placing values 04, 64, 40 and 48 to intcRegs->INTMUX1 register.

     

    The C6747 only has 12 hardware interrupts however there are 128 events that can generate an interrupt. The interrupt selector determines which of the 128 events can  actually generate an CPU interrupt. Inside the interrupt selector are interrupt mux registers (INTMUX) that map the source for each of the 12 available CPU interrupts.