Part Number: TMDS64GPEVM
Other Parts Discussed in Thread: AM6442
Hello
For our custom product based on AM6442 I we want to switch to the kernel 6.1. I switched to the newest meta-ti layer and in yocto recipes I set
PREFERRED_VERSION_virtual/kernel = "6.1"
PREFERRED_PROVIDER_virtual/kernel = "linux-ti-staging-rt"
and the image was built successfully. I see that also u-boot was updated to 2023 version. After flashing SD card the booting process hangs. I see only below logs and nothing happens.
U-Boot SPL 2023.04-g17439dc59a (Sep 26 2023 - 15:26:19 +0000)
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed -121
Resetting on cold boot to workaround ErrataID:i2331
Please resend tiboot3.bin in case of UART/DFU boot
resetting ...
U-Boot SPL 2023.04-g17439dc59a (Sep 26 2023 - 15:26:19 +0000)
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed -121
SYSFW ABI: 3.1 (firmware rev 0x0009 '9.0.5--v09.00.05 (Kool Koala)')
SPL initial stack usage: 13376 bytes
BR
Jakub